EN
Country: EN (Austria)
Select country/region

Language

  • German
  • English
stage-teaser-component io-link-overview-image

IO-Link

Communication interface for efficient integration of sensor data into the automation network.

IO-Link in automation technology

IO-Link is a communication interface used in automation technology to connect sensors and actuators with higher-level systems. Thanks to the innovative technology, sensors and actuators become active process participants, which opens up new possibilities in communication between devices and the system controller. IO-Link enables efficient and flexible automation – across all industries.

IO-Link product portfolio

There are many reasons for using IO-Link. Regardless of the level of integration, there are numerous advantages. SICK offers a wide range of IO-Link devices, IO-Link masters, and digital solutions for the further processing of generated process data.

SICK sensor solutions with IO-Link functionality

WHAT OUR CUSTOMERS ARE SAYING

The use of IO-Link sensors significantly increases our machine availability. We can react flexibly and quickly to changing packaging so that the sensors are always optimally matched to the objects. The IO-Link technology has impressed us and we will continue to rely on IO-Link products from SICK in the future.
Michael Huber Product Development TPP, MULTIVAC Sepp Haggenmüller SE & Co. KG

ADVANTAGES

Digitalization and transparency down to the lowest field level.

Simple integration

Simple integration

As a globally standardized technology, IO-Link makes it easy to integrate the intelligence of sensors and actuators into automation systems.

High compatibility

High compatibility

IO-Link is a free standard and offers seamless integration into other systems as well as a high level of flexibility for application-specific adaptations.

Reduction of downtimes

Reduction of downtimes

IO-Link ensures an efficient, fail-safe transmission of data and enables meaningful conclusions to be drawn so that maintenance work can be planned predictively.

Cost savings

Cost savings

Extensive parameterization options via IO-Link keep the sensor variance low, which reduces costs. In addition, the cabling effort and associated costs are lower.

MORE INFORMATION ON IO-LINK

CONTACT US!

Are you interested in application solutions from SICK? Our experts will be happy to help you and find the right solution for you.

Contact via email

Contact

IO-LINK APPLICATION EXAMPLES

Production environment in which cabling has been reduced through the use of IO-Link

Simple reduction of cabling effort

In a production plant, multi-story warehouses supply production components. A large number of sensors are used for this. IO-Link bundles the signals from the sensors and transmits them with significantly lower cabling effort.
 

SICK sensor with signal lamp

Intelligent visualization of operational statuses

No complex control system is required to display a fill level. Both the distance sensor and the signal lamp are connected directly to the IO-Link master with SIG300. The simple logic is set up directly in the logic editor of the IO-Link master – no special expertise is required.

SICK employee standing with laptop in a production environment

Reduction of downtimes through predictive maintenance

When combined with an ERP system in the cloud, the strengths of IO-Link-capable devices really come into their own. Process-relevant variables or internal device parameters are continuously monitored and transferred to the cloud. Unplanned downtimes can thereby be easily avoided.

To the IO-Link application examples

GENERAL INFORMATION ON IO-LINK