EN
Country: EN (Austria)
Select country/region

Language

  • German
  • English
stage-teaser-component io-link-applications-image

IO-Link application examples

Efficiency and flexibility regardless of the level of integration.

Optimize production processes through the use of IO-Link

IO-Link is a standardized communication protocol for simply and efficiently integrating sensors and actuators into automation technology. Regardless of the level of integration, it opens up numerous application possibilities to improve the efficiency and flexibility of production processes.

IO-LINK APPLICATION EXAMPLES AT THE FIELD LEVEL

Reduction in cabling effort

In a production plant, multi-storey warehouses are used to supply production components. The handling units are equipped with a large number of binary switching sensors to monitor the end positions, the aisles, and the load. 

The sensor signals are bundled via IO-Link-capable sensor hubs and connected to the controller via an IO-Link master using a fieldbus. Depending on the variant, over 100 binary sensors can be connected to an IO-Link master in this way. In this application example, the use of IO-Link already offers the following advantages at the field level:

Increased efficiency and cost savings:

  • Reduction in installation work and material costs 
  • Avoidance of wiring errors thanks to the consistent use of standardized plug connections

Components for this application example:

Production environment with reduced cabling

Visualization of operational statuses

The fill level of a production system is precisely recorded via IO-Link-capable sensors and visualized via a signal lamp. The distance sensor and the signal lamp are connected directly to the IO-Link master for this purpose. It has logic modules that create the required signal processing logic and derive output signals. The logic modules are accessed via an integrated web server. The use of IO-Link results in the following advantages for this application example:

Simple programming and cabling:

  • Simple programming of the logic modules without specialist knowledge
  • Easy installation, even in confined spaces, as the devices do not require their own voltage supply
  • Option of condition monitoring via the cloud with integrated REST interface

Components for this application example:

Tanks in production environment with signal lamp

IO-LINK APPLICATION EXAMPLES AT THE CONTROL LEVEL

Optimization of system development

In practice, sensors are generally not operated with the factory default settings, but are parameterized for the specific use via the controller. In particular, the integration of IO-Link into the control level via a controller (PLC) offers the following advantages:

Simple commissioning and predictive maintenance:

  • Fast setup of series machines and reduction of device variance thanks to automated parameter download from the controller (PLC)
  • Plug-and-play replacement of sensors incl. parameterization during operation
  • Avoidance of incorrect sensor parameterization thanks to the ability to reproduce device settings on a large number of sensors
  • Provision of sensor parameters for predictive maintenance and the option of proactive notification if defined limit values are exceeded or not reached

Components for this application example:

SICK employee parameterizes sensors via a tablet

IO-LINK APPLICATION EXAMPLES AT COMPANY LEVEL

Reduction of downtimes

Thanks to IO-Link and the integration of available sensor data into the cloud, the productivity of systems can be monitored over any distance. IO-Link integration offers the following advantages at the company level:

Fast detection of critical states and long-term trends:

  • Transmission of status information for early detection of any failures or critical states
  • Predictive maintenance based on continuous monitoring of process-relevant parameters
  • Central processing of remote parameter sets by transmitting data to the cloud

Components for this application example:

SICK employee standing with laptop in a production environment

CONTACT US!

Are you interested in application solutions from SICK? Our experts will be happy to help you and find the right solution for you.

Contact via email

Contact