Data processing information Sentio Creator

SICK vous remercie de votre visite sur nos sites Internet et de votre intérêt pour nos entreprises, nos produits et nos services. La protection de votre vie privée est notre priorité et nous souhaitons que vous vous sentiez en sécurité lorsque vous naviguez sur nos sites Internet. C'est pourquoi nous tenons à vous expliquer quelles sont les informations que nous traitons lors de votre visite sur nos sites Internet.

Data controller SICK AG, Erwin-Sick-Straße 1, 79183 Waldkirch, Germany
Purpose of processing SICK may use the data we collect to provide you with rich, interactive experiences. We may use data to:
  • Provide our products, which includes updating, securing, and troubleshooting, as well as providing support. It also includes sharing data, when it is required to provide the service or carry out the transactions you request.
  • Improve and develop our products.
  • Personalize our products and make recommendations. We also use the data to operate our business, which includes analyzing our performance, meeting our legal obligations, developing our workforce, and doing research. Improving the usability and the user experience of Sentio Creator.
Categories of data Sentio Creator collect data, such as program crashes, errors and usage data. The collected data is anonymous and non-personal. The collected data varies based on the error. It may contain stack traces and exception information. Diagnostic information when a tool crashes or errors occur to help understand why the crash or error occurred and what changes are needed to prevent the crash or error in the future.

In some cases, the Windows user name may be saved as part of a file or directory path. This information is not actively evaluated and is used exclusively for technical error analysis. Usage data collects information about how features are used and perform which helps SICK prioritize future product improvements.

Device status data:
In connection with firmware installations, technical device status data may be processed. This includes, for example, operating hour counters, the number of device restarts, temperature readings, diagnostic information, and information about the status of components and assemblies. This data is used exclusively for technical purposes, in particular for error analysis, to ensure proper operation, and for the further development of our products. The data is not personally identifiable.
Legal basis Consent
Consequences of failure to provide the data SICK ID: If you do not log in with your SICK ID, no software such as extensions for the Sentio Creator can be installed. This also includes firmware packages and similar additional functions.

Data for analysis purposes: No consequences
Retention time We do not store any personal data.
Data source We only process personal data provided directly by you.
Transmission to third countries We do not transfer personal data to third countries.
Logic of automated decision-making We do not perform any automated decision-making.

Vos droits

Vous avez le droit

  • d’obtenir des renseignements sur les données personnelles vous concernant ;
  • de rectifier des données personnelles vous concernant ;
  • de supprimer ou de bloquer des données personnelles vous concernant ;
  • de vous opposer au traitement des données personnelles vous concernant ;
  • de transférer des données personnelles vous concernant ;
  • de révoquer votre consentement avec effet ultérieur dans la mesure où le traitement des données personnelles vous concernant repose sur votre consentement ; ainsi que
  • de porter plainte auprès d’une autorité de surveillance de la protection des données si vous estimez que le traitement des données personnelles vous concernant enfreint la législation sur la protection des données.

Pour ce faire, veuillez vous adresser à notre responsable de la protection des données. Nous répondons à toutes les demandes.

SICK AG
Responsable de la protection des données
Erwin-Sick-Strasse 1
79183 Waldkirch
Allemagne

datenschutz@sick.de

Modification de la déclaration de confidentialité

Nous nous réservons le droit d’adapter à tout moment la déclaration de confidentialité aux exigences en vigueur. La déclaration de confidentialité actuelle peut être consultée à tout moment sur nos sites Internet.