EN
Country: EN (Austria)
Select country/region

Language

  • German
  • English
digitalsolutions-quality-woodprocessing-stage-teaser-image

Automated image processing optimizes wood processing:

Higher yield and optimum reliability

The challenge is that natural and organic materials such as wood are difficult to classify manually

Even conventional rule-based machine vision image processing reaches its limits here. Inspections are time-consuming and costly, and they vary in accuracy. Wood-processing plants need reliable systems for procedures such as orienting wood boards in such a way that they do not deform over time, which can happen if the annual rings are not positioned in opposing directions.

Using the InspectorP62x 2D vision camera combined with the Intelligent Inspection SensorApp, manufacturers can automate processes, shorten inspection times and increase their yield. The vision camera estimates the orientation of wood boards according to their annual year ring pattern. This is done with input from a trained deep learning network that is deployed directly on the camera and configured by the Intelligent Inspection SensorApp. Orienting wood boards is then fully automated, ensuring that further processing proceeds in the correct orientation.

Benefits:

Consistent quality is a given, and error-prone, time-intensive manual inspection a thing of the past. Automated inspection optimizes reliability and scalability: Manufacturers can scale production as needed while maintaining the same high level of quality control. And reducing inspection costs and optimizing production improves profitability.

People standing at screens observing the process

THESE COMPONENTS ARE PART OF THE SOLUTION

Intelligent Inspection SICK SensorApp

2D machine vision solution powered by deep learning

The deep learning-powered Intelligent Inspection toolset from SICK enables powerful anomaly detection and object classification that is not possible with rule-based machine vision. 

CONTACT US!

Do you have any questions about our digital solutions, are you interested in a use case, or would you like to make an appointment with our local expert?

Contact via email

Contact