Light off, spot on: laser sensors for any application

2021 Oct 20

A bundled light beam reveals the protagonists in the dark – or presents them in the best light figuratively speaking. What works on the stages of this world offers something of a blueprint for the many product families of laser sensors at SICK. With their bundled light, the many different laser sensors safely and reliably detect and record either objects or the surroundings, depending on the application – even independent of ambient light and other challenges.

precise laser scanner
precise laser scanner

The competing systems for reliable object detection are LED and laser based solutions. Laser sensors have a clear advantage, however: compared to LED sensors they offer significantly longer sensing ranges, a higher precision, and a sharply defined diameter of the light cone. Consequently, the light spot always has a sharp contour and is easily recognizable within the visible spectrum range, and the light spot remains small relative to the working distance. This enables laser sensors to safely detect even the smallest objects, for example needles and threads. A further advantage in certain applications is that the laser sensors can detect objects through holes or narrow openings.

precision is the source of good performance
precision is the source of good performance

Precision is the source of good performance

A sensor should not squint. That might sound strange, but we refer to a so-called squint angle when installing the optoelectronic module and while adjusting the laser diode. The diode is aligned by a fully automatic gripper and using an alignment target until the squint angle is almost eliminated, and is then glued to the module. This works consistently from sensor to sensor thanks to micrometer-precise monitoring by a camera system in this automatic manufacturing process. This ensures that all laser sensors of the same type leave the factory, in principle, identically adjusted – a repeatability that makes initial mounting and also supplementing or replacing the sensor significantly easier.

Not all lasers are the same

While the housings often look identical, they contain two different technologies depending on the application requirements. Neither is better or worse than the other, but simply the most suitable for the particular application. There are therefore laser sensors based on triangulation, and ones based on time-of-flight (ToF).

Triangulation – thinking laterally

Laser photoelectric proximity sensors with background suppression measure distances by calculating angles (triangulation). The emitted light is reflected by an object and hits the receiver element at a certain angle depending on the distance. Based on the position of the light spot on the receiver element, it is possible to determine the distance of the object. This measurement principle has two advantages. Firstly it allows you to configure a precise background suppression that can be used, for example, to reliably detect flat objects on a conveyor belt. Secondly, it enables even very close objects to be detected because the triangulation principle has virtually no geometrical blind areas. This principle of operation has certain limits, however, that are reached in particular in the case of very dark, weakly reflecting surfaces.

time of flight laser scanner
time of flight laser scanner

Time of flight – it doesn’t get any faster than this

In the case of a time-of-flight photoelectric proximity sensor, on the other hand, the object color is almost irrelevant. This sensor does not measure optical angles, but rather the time-of-flight of laser light. The sensor emits laser pulses and measures the time until the reflected light arrives at its receiver element. This measurement principle is therefore almost independent of the optical reflectance behavior of an object. At the same time it is also extremely impervious to optical interference by reflections, ambient light or artificial light. ToF laser sensors also deliver stable detection results even at large detection angles. Furthermore, ToF laser photoelectric proximity sensors are so smart that they can deliver a continuous distance signal and also make it available via an analog output or IO-Link. Laser sensors are designed to be smart sensors. They can therefore be used to implement Industry 4.0 applications such as condition monitoring in order to make automation networks more efficient and future proof.

huge range of different applications
huge range of different applications

Huge range of different applications

The different measurement principles of laser sensors also suggest their possible applications. From laser scanners that detect ultra small nearby objects right through to photoelectric sensors with a detection range of up to 60 meters – a huge spectrum. And this applies, of course, to all industries, whether it be packaging machine construction, the automotive and supply industry, the electronics or solar industry – laser photoelectric sensors provide reliable and economical solutions to automation tasks in many areas. This include high-precision and reproducible applications for position, presence, overrun and height checking. And new and modified versions are continuously being released. The photoelectric sensors in the G6L product family, for example, will impress you across the board with both their standard mounting configuration of 1-inch spaced holes and also their functional characteristics. And the MultiTask photoelectric sensors in the PowerProx range have now been extended by the high performance WTT4SL in a miniature housing – for maximum flexibility in machine design. Thanks to the high energy density and convergence of the laser beam, the various laser sensors can master even the most demanding ambient conditions where LED sensors often reach their limits. So we can clearly say: spot on for the winner.

Read more

Detection what ever circumstances

Read more

Transparent advantages: photoelectric sensors in heavy-duty operation

Read more

The W16 and W26 product families a new generation of SICK photoelectric sensors

Read more