Privacy policy for the development of a camera system for detection of persons

SICK, internet sayfalarımızı ziyaretinizden ve şirketimiz, ürünlerimiz ve hizmetlerimize göstermiş olduğunuz ilgiden dolayı mutluluk duyar. Özel hayatınızın korunması bizim için çok önemlidir ve internet sayfalarımızı ziyaret ederken kendinizi güvenli hissetmenizi istiyoruz. Bu amaçla, internet sayfalarımızı ziyaretiniz sırada hangi bilgileri işlediğimizi size aşağıda açıklıyoruz.

Responsible SICK AG, Erwin-Sick-Straße 1, 79183 Waldkirch, Germany
Purpose of processing Development and validation of a system for safeguarding hazardous areas
Categories of data
  • Image data
  • Video data
  • 3D information
  • Time of recording
  • Identification of the recording unit
  • Camera settings
  • Diagnostic information
The quality of the video material allows people to be identified in particular, but not exclusively, when the person's gaze is directed towards the camera system.
Legal basis GDPR Art. 6 (1) f) - legitimate interests
Legitimate interest SICK processes image, video and 3D data in combination with the above-mentioned additional information for the training and validation of AI systems and for the validation of deterministic algorithms. Most of the data is processed automatically. This processing is done to protect people in the vicinity of machines and to prevent accidents involving them. By developing such a system for the protection of persons, there is a justified corporate interest in the general welfare of all persons. The purpose of the system's accident prevention therefore means that future protection in the interests of all people outweighs the right to the image recordings of the individual, which is worthy of protection.
Consequences of failure to provide the data None.
Storage duration On the basis of the data, the accuracy and robustness of the product are to be assessed and improved over the product life cycle. In order to comply with product liability in accordance with §13 para. 1 ProdHaftG, the recorded data is stored for 10 years after the last sale of a system based on this technology.
The data subject may object to the processing of personal data within one week, specifying the time and place of recording. In this case, SICK will delete the data.
Data source Direct collection of data through image / video recording.
Recipients of the data Certifying bodies
Transmission in third countries For manual completion and to check characteristics, the data is transmitted to a subsidiary of SICK AG in Vietnam. The data is displayed there and characteristic information is supplemented or corrected, but the data is not stored.
Logic of the automated decision We do not make automated decisions that may have consequences for data subjects.

 

Haklarınız

Aşağıdaki haklara sahipsiniz

  • Sizinle ilgili kişisel veriler hakkında bilgi edinme;
  • Sizinle ilgili kişisel veriler hakkında bilgilendirilme;
  • Sizinle ilgili kişisel verileri silme veya engelleme;
  • İlgili kişisel verilerin işlenmesine itiraz etme;
  • Sizinle ilgili kişisel verilerin aktarılabilirliği;
  • Sizinle ilgili kişisel verilerin işlenmesinin kendi onayınızı ihlal etmesi durumunda, verdiğiniz onayı gelecekte yürürlüğe girmek şartıyla geri çağırma ve
  • Sizinle ilgili kişisel verilerin işlenmesinin veri koruma yasasını ihlal ettiğini düşünmeniz durumunda, bir veri koruma denetim makamına şikayette bulunma.

Bu amaçla lütfen veri koruma görevlimize başvurun. Tüm soruları uygun şekilde yanıtlayacağız.

SICK AG
Datenschutzbeauftragter
Erwin-Sick-Straße 1
79183 Waldkirch
Almanya

datenschutz@sick.de

Veri koruma beyanında değişiklik

Veri koruma beyanını, yürürlükteki istemlere her zaman uyarlama hakkını saklı tutuyoruz. Güncel veri koruma beyanı, internet sayfalarımızdan her an çağrılabilir.