Mobile robots from SHERPA MOBILE ROBOTICS boost mobility and productivity

2023. 1. 17

Integrating mobile robots that work safely in the immediate vicinity of operators and machines – that is the aim of SHERPA MOBILE ROBOTICS (SMR). The autonomous and mobile robots allow diverse solutions: for example making work operations easier or automating the transfer of a load from A to B, thereby boosting mobility and productivity.

Mobile robots that work safely in the immediate vicinity of operators and machines - that is the goal of SHERPA MOBILE ROBOTICS
Mobile robots that work safely in the immediate vicinity of operators and machines - that is the goal of SHERPA MOBILE ROBOTICS

 

High safety requirements for users

SHERPA MOBILE ROBOTICS offers its customers a whole range of solutions. Their first two customizable autonomous mobile robots (AMR) provide customers with solutions for absolutely every scenario. The first AMR transports pallets and has a load bearing capacity of up to one tonne, the second transports containers.

SHERPA MOBILE ROBOTICS offers a whole range of solutions for its customers.
Perfectly prepared for any scenario - the individually adaptable Autonomous Mobile Robots.
SHERPA MOBILE ROBOTICS offers a whole range of solutions for its customers.
Perfectly prepared for any scenario - the individually adaptable Autonomous Mobile Robots.

Safety was the top priority for the developers. To ensure the highest level of safety for the robot in its environment, SHERPA MOBILE ROBOTICS approached SICK. Laurent Troesch, R&D at SMR, explains the background of the collaboration: “Initially we envisaged an architecture for the safety functions that used non-certified components (sensors, controllers, etc.) even through we were aiming for Performance Level d for most of them. We quickly noticed that such an approach would be very complex and time-consuming, which would not allow the speedy market launch of a reliable series of robots.

Furthermore, tailored solutions such as this are rather inflexible and are not particularly suitable for upgrading or use in future robot series. In developing our robots, we were looking instead for efficient and flexible solutions that can be quickly integrated. The exchange of ideas and support from SICK helped us a lot with this.”

Safety is always a top priority for the developers.
SHERPA products move absolutely safely even in sometimes confined environments.
Safety is always a top priority for the developers.
SHERPA products move absolutely safely even in sometimes confined environments.

Stéphane Rauline, Technical Sales Engineer at SICK France took on the challenge from SMR and got the collaboration between the two teams going. The engineers at SMR were looking for safety laser scanners and safety encoders. They therefore decided to go with the S300 safety laser scanner and the DFS60S safety encoder. For the SHERPA-P, they are using the nanoScan3 safety laser scanner and the Flexi Soft Drive Monitor safety controller. This enables the SHERPA products to move about with absolute safety even in sometimes confined surroundings.

 

안전 레이저 스캐너
SICK의 가장 작은 안전 레이저 스캐너 – 엄청난 내구성과 높은 정밀성
nanoScan3
안전 제어기
소프트웨어로 프로그래밍이 가능한 안전 제어기
Flexi Soft
인크리멘털 엔코더
안전한 움직임 감시를 위한 안전 엔코더
DFS60S Pro

 

Competent and flexible support

Jeffrey Yannou, mobile applications expert at SICK France, was responsible for supporting SHERPA throughout the entire project. Thanks to this collaboration, a quick market launch was achieved. Renowned companies such as Siemens, Airbus, Fnac, Darty, and FPT Industrial are already using SHERPA robots. FPT (Fiat Powertrain Technologies) Industrial in Bourbon-Lancy in the department of Saône-et-Loire is even using a whole fleet of mobile robots from SHERPA. The mobile robots are making assembly tasks easier and reducing the risk when transporting loads. Their smooth operation is also boosting productivity.

Thanks to the cooperation between SHERPA and SICK, a rapid market launch was achieved.
Thanks to the cooperation between SHERPA and SICK, a rapid market launch was achieved.
Thanks to the cooperation between SHERPA and SICK, a rapid market launch was achieved.
Thanks to the cooperation between SHERPA and SICK, a rapid market launch was achieved.

Another advantage of SHERPA robots is that they can move safely between operators, manned forklift trucks, and AGVs. “Thanks to the integration of six robots we have gained concrete experience in fleet management in a real-life environment. We will be able to apply this new knowledge for customers who are already waiting for this type of technology,” explains Damien Winling, Technical Director at SMR.

This is only the beginning of a big adventure for SHERPA and its mobile robots. They are putting their trust in the latest technologies from SICK that make the mobile robots even more efficient and safe. A shared journey for both companies that has only just begun.

 

Read more

Safety laser scanner technology enables mobile robots to navigate work environment safely

Read more

Ultracompact mobile robots optimize the process chain

Read more

Autonomy and flexibility in intralogistics – the road is clear for automated guided vehicles

Read more

더 궁금한 것이 있으신가요?

저희 전문가에게 문의하세요

이동식 로봇:
Move into new dimensions

생산, 물류, 서비스를 막론하고 도입되는 로봇 시스템. 모든 종류의 이동식 로봇을 위한 센서 솔루션

더 알아보기