Encoder – invisible helper for automation

2025/05/20

To get things moving with automation, something also needs to move – automatically – in machines and systems. Movement alone is not sufficient, however. Robots, tool and packaging machines, industrial trucks and conveyor systems, for example, only function as desired if their movements are performed in a controlled, monitored and reproducibly safe manner. Encoders – often invisible in electrical drive systems – take care of precisely this task. They ensure that machine movements in automated systems can be reliably controlled.

Bewegungssteuerung – das ist es, wofür Encoder eingesetzt werden.
Bewegungssteuerung – das ist es, wofür Encoder eingesetzt werden.

Motion control – that is what encoders are used for. They record – as linear or rotary measurement systems – positions, displacements, speeds and directions of rotation. Using these parameters, it is possible to uniquely define – and therefore also control – movement sequences in most cases in industrial automation. Only then can robots accurately grip and put down objects, tools and fixtures be precisely positioned in machines, and conveyor systems and vehicles reliably perform transport tasks.

 

The requirements on encoders are increasing

Their measurement function alone is no longer enough, however. With automation performance increasing, machines becoming every more compact, the quality requirements on processes and product becoming more stringent, and the ongoing move towards digitalization and networking, encoders need to offer more. Their space-saving design and mechanical variability in regard to the shaft and connection technologies are just as much in demand as their support for shorter and more precise machine cycles, which enables production rates to be increased while at the same time minimizing errors and ensuring quality.

This, in turn, requires a correspondingly fast data transmission between encoders and automation systems – ideally in real time and synchronously via PROFINET IRT. The control-related integration with the help of tried-and-proven tools should be just as easy as the provision of diagnostic data for condition-based machine and system maintenance. All these customer expectations have now made encoders a high tech component in kinematic automation – in particular when it comes to optimizing the efficiency of machines through precise motion control while transmitting data synchronously via fieldbus in real time and in a future proof manner.  

Das Encoder-Portfolio von SICK hält eine große Zahl linearer, rotativer und berührungslos messender Lösungen für die Bewegungssteuerung bereit.
The encoder portfolio from SICK provides a large number of linear, rotary and non-contact measurement solutions for motion control.
Das Encoder-Portfolio von SICK hält eine große Zahl linearer, rotativer und berührungslos messender Lösungen für die Bewegungssteuerung bereit.
The encoder portfolio from SICK provides a large number of linear, rotary and non-contact measurement solutions for motion control.

 

All-rounders are rare – but one does exist 

High-end automation, as demanded by innovative machine builders and end-users in particular, requires encoders that can excel in all disciplines. These kinds of all-rounders are currently still rare, though, and consequently in much demand. They are readily available, however, in the encoder portfolio of SICK thanks to the new ANS/ANM58 PROFINET absolute encoder generation, which has been designed through and through for high machine and system productivity. The improved optical measurement system that SICK developed and manufactures in-house enables high-precision motion control, while the real-time transmission of movement and position data enables short cycle times and PROFINET IRT synchronous processes.

 

The compactness is best-in-class: At just 39 mm, the sensor variant with radial connection has the smallest installation depth of all encoders of this type on the market. A further plus is the many mechanical variants of the product, with a flat and narrow design, three different shaft options, and axial or radial plug variants to choose from. These two features together offer significant advantages when mechanically integrating the device in tight and demanding installation situations. Control-related integration is simple via the Siemens TIA-Portal, while configuration of the encoder parameters can also be carried out via the SICK Engineering-Tool SOPAS.

アブソリュートエンコーダ
PROFINET IRT対応の高分解能アブソリュートエンコーダ
ANS/ANM58
Die neue Absolut-Encoder-Generation ANS/ANM58 PROFINET wurde konsequent auf höhere Maschinen- und Anlagenproduktivität ausgelegt.
The new ANS/ANM58 PROFINET absolute encoder generation has been designed through and through for higher machine and system productivity.
Die neue Absolut-Encoder-Generation ANS/ANM58 PROFINET wurde konsequent auf höhere Maschinen- und Anlagenproduktivität ausgelegt.
The new ANS/ANM58 PROFINET absolute encoder generation has been designed through and through for higher machine and system productivity.

 

Comprehensive condition monitoring integrated

Besides highly precise measurement data for motion control, the ANS/ANM58 absolute encoders also provide relevant diagnostic data from the machine process. With data on temperatures, speeds, cycles, counters or timestamps as well, they support condition-based system maintenance. This diagnostic data can also be used to configure application-specific limit values, using which warning thresholds for targeted maintenance and servicing measures can be set up. This makes it possible to monitor process performance, avoid unplanned machine downtimes, and increase the productivity of systems. In this way, the rotary singleturn and multiturn sensors fully cover the wide range of industrial requirements on state-of-the-art encoders.

Die große mechanische Varianz des ANS/ANM58 PROFINET bietet erhebliche Vorteile bei der Integration in anspruchsvolle Einbausituationen.
The availability of many mechanical variants of the ANS/ANM58 PROFINET offers substantial advantages when integrating the device in demanding installation situations.
Die große mechanische Varianz des ANS/ANM58 PROFINET bietet erhebliche Vorteile bei der Integration in anspruchsvolle Einbausituationen.
The availability of many mechanical variants of the ANS/ANM58 PROFINET offers substantial advantages when integrating the device in demanding installation situations.

 

A particular focus on: packaging technology, machine building and storage and conveying technology

Exact position, displacement, speed or acceleration data and their real-time transmission is essential for reliable and reproducible precision movements, safe processes as well as more efficiency and productivity for drives and axes. That is why the ANS/ANM58 absolute encoder generation is used, for example, in the packaging technology of processes requiring high synchronicity. The new encoder generation is proving itself in machine building as a means of reproducibly recording positions and measuring movements for precise machine and system control. In storage and conveying technology, it is used for the efficient automation of transport and handling processes.

 

その他の記事

When an encoder becomes the safety standard

Read more

Constant monitoring of film webs so that nothing goes wrong

Read more

Continuous monitoring of the foil webs: so nothing goes wrong

Read more