Reduction of greenhouse gases in the waste management industry

Apr 22, 2024

The waste management industry also needs to reduce its global greenhouse gas emissions. A large proportion of the waste produced globally – controlled or uncontrolled – continues to go to landfill.

Waste incineration facilities are part of the biogenic carbon cycle, emitting a mixture of biogenic and fossil CO2. Burning fossil fuels releases carbon that has been locked up in the ground for millions of years, while burning biomass emits carbon that is part of the biogenic or bio-based carbon cycle

Welcome to part six of our series on decarbonization where we focus on waste management.

A large proportion of the waste produced globally continues to go to landfill.
A large proportion of the waste produced globally continues to go to landfill.

Reduction in methane emissions through recycling and thermal treatment

Landfill sites emit a significant amount of methane (CH4), a greenhouse gas that is 25 times more harmful to the environment than carbon dioxide (CO2). To achieve the net zero goal, the methane emissions from landfill need to be eliminated as far as possible. This is possible through holistic recycling and the thermal treatment of non-recyclable materials. Germany and several other European countries are successfully doing this thanks to high recycling rates and an effective network of thermal treatment plants.

Graphic of an integrated resource recovery facility.(1)
Graphic of an integrated resource recovery facility.1
Graphic of an integrated resource recovery facility.(1)
Graphic of an integrated resource recovery facility.1

Sensor solutions for holistic recycling

We need raw materials for almost everything: houses, roads, vehicles, entertainment media. But raw materials are a finite resource. In a sustainable circular economy, prevention, recycling, energy recovery, and the reliable avoidance of waste and removal of pollutants are of the utmost priority. This enables secondary raw materials to be made available to the economy again and conserves natural resources. The waste is tracked, controlled, sorted and recycled. Numerous sensors are used for this.

Bottles on conveyor belt scanned by a SICK sensor.

Conveyor belts transport waste within the recycling facility. Malfunctions of the conveyor belts can lead to significant delays and involve major costs. It is therefore necessary to monitor the operation of all conveyor belts, as well as the proper loading, unloading, and positioning of materials. The DFS60 incremental encoder provides the information on transport speed, while the Bulkscan® LMS511 flow sensor determines the volume flow, center of gravity of the load, and load height contactlessly and with no wear-and-tear

增量型編碼器
適合高要求應用的高解析度可程式設計型增量型編碼器
DFS60
流量感測器
採集體積流量狀態,免接觸且無須維修
Bulkscan
Malfunctions of the conveyor belts can lead to significant delays and involve major costs.
Malfunctions of the conveyor belts can lead to significant delays and involve major costs.
Malfunctions of the conveyor belts can lead to significant delays and involve major costs.
Malfunctions of the conveyor belts can lead to significant delays and involve major costs.

Energy recovery from non-recyclable materials

The energy produced in the thermal treatment plants is fed to the public supply network in the form of district heat and electricity. The energy is also further processed directly on site into alternative fuels such as hydrogen.

 

Example: Continuous emission monitoring of all pollutant components in the exhaust gas

To reduce emissions, the exhaust air in various processes is cleaned. Intelligent sensor solutions from SICK enable the exhaust air cleaning systems to combust the air effectively and operate optimally.

Sensor solutions from SICK enable the exhaust air cleaning systems to combust the air effectively and operate optimally.

Continuous emission measurement systems (CEMS) such as the MCS200HW or MCS100FT simultaneously measure up to twelve pollutant components of the exhaust gas and reliably monitor the limit values. The MERCEM300Z gas analysis system measures mercury in the raw and clean gas. Dust concentrations are reliably determined by the DUSTHUNTER dust measuring devices, and flow volumes by the FLOWSIC100 gas flow meters

The MEAC300 data acquisition system is responsible for recording, saving, normalizing, analyzing, displaying, and forwarding the emissions data.

數位分析儀解決方案
流量量測儀
The condition data of the analyzers is visualized and interpreted in real time with the help of Condition Monitoring.
The condition data of the analyzers is visualized and interpreted in real time with the help of Condition Monitoring.
The condition data of the analyzers is visualized and interpreted in real time with the help of Condition Monitoring.
The condition data of the analyzers is visualized and interpreted in real time with the help of Condition Monitoring.

The condition data of the analyzers is visualized and interpreted in real time with the help of Condition Monitoring. Any significant changes in the analyzers are displayed and, if required, visualized concisely and clearly in a browser-based dashboard. Solutions and recommended actions are displayed in direct form. The Monitoring Box enables operators of waste incineration plants to implement digitally-supported predictive maintenance. This increases the machine and plant availability and reduces the costs for unplanned service deployments.

 

CCUS in the waste management industry

Initial pilot plants for carbon capture already exist. Around 50% of the waste from thermal treatment plants are biogenic materials. Through the capture and treatment of CO2 from fossil and biogenic waste, these plants can achieve a negative CO2 footprint. Gas analyzers, dust concentration measurement systems, and flow metering systems from SICK are used in carbon capture utilization and storage

 

Biogenic CO2 measurement: the main reasons

Emission Trading Systems (ETS) like EU ETS, UK Environment Agency’s Pollution Inventory Guidance, German BEHG and China Certified Emission Reduction (CCER) are in operation. All laws differ between fossil and renewable carbon. 

Thermal waste treatment facilities with Carbon Capture units will provide a major contribution of negative CO2 emissions due to the biogenic portion of the heterogeneous feedstock. Net zero GHG emissions are only achievable with significant negative CO2 emissions balancing the remaining GHG (e.g. from agriculture). Knowing the negative CO2 emissions with best possible accuracy is desired. For further utilization of captured CO2 the green portion is important for ecological, bio-based evaluation. Furthermore, the renewable share of the recovered energy by Waste-to-Energy plants is of high public interest.

In some European cities the management of waste per capita is based on the fossil portion. Also for this purpose the determination of the fossil and biogenic CO2 fractions is required

For these reasons SICK started the cooperation with Genius5-Instruments GmbH for worldwide sales and service of the PmCTrace biogenic CO2 measurement system, a future part of CEMS in waste incineration plants.

 

Source

1https://eswet.eu/recovering-the-non-recyclable-the-integrated-resource-recovery-facility/

 

Read the other parts of our series on decarbonization

Low-carbon combustion and production processes

Read more in part one of our series on decarbonization

Decarbonization: gas analysis and flow measurement for transfer and process applications

Read more in part two of our series on decarbonization

Decarbonization in the energy sector

Read more in part three of our series on decarbonization

Decarbonization in shipping and air transport

Read more in part four of our series on decarbonization

Decarbonization approaches in mining and metal production

Read more in part five of our series on decarbonization

The products
featured in this
article are now
supplied by Endress+Hauser.

Click here for the products on endress.com