A head of steam: industrial instrumentation solutions for boilers

2020 Sep 21

From the first industrial revolution to the fourth, inspirational change has been driven by a willingness to embrace the unconventional and cross-traditional industry boundaries. A partnership between one of the UK’s oldest and best-known boiler manufacturers, Byworth Boilers with SICK, has helped fine-tune its boiler house controls to save up to 7% on customer fuel bills.

At its heart is the industrial boiler, a process-critical workhorse that must always be completely reliable.
At its heart is the industrial boiler, a process-critical workhorse that must always be completely reliable.

 

Heroic and historic, steam has always had the power to inspire

It remains one of the most effective and efficient ways of transporting and delivering heat for modern industrial processes. At its heart is the industrial boiler, a process-critical workhorse that must always be completely reliable. With brands like Yorkshireman, Dalesman and Fellsman, Byworth’s boilers conjure up a nostalgic picture of more than 50 years as a family firm. Yet, throughout its history, the company has consistently demonstrated an insatiable appetite for innovation. With an agile approach to problem solving, its competitive advantage has been protected by a commitment to continuous improvement; reducing customers’ fuel use, increasing operating efficiency and minimising downtime.

In early 2020, Byworth Boilers will open a £2 million extension to its manufacturing headquarters in Keighley, West Yorkshire, in the UK. From small boilers to service the rush of new micro-distilleries, to leviathans for hospitals and animal feed mills, Byworth’s business is built on long-term customer partnerships.

 

Industrial boilers are energy hungry

Measurement and control are the means to get every last drop of fuel efficiency, by keeping every element of pressure, level and temperature in perfect balance. Byworth’s Research and Development is centred on a fully operational boiler room at the Keighley site, where the latest available instrumentation technology is carefully evaluated before being applied on customer systems.

Byworth’s relationship with SICK has grown from initial Research and Development trials of a simple pressure switch to the point where Byworth has standardized on SICK instruments for various processes across its boiler ranges. SICK’s PBS pressure transmitter, LFP guided wave radar level sensor, TBS temperature switch and DOSIC ultrasonic flowmeter, are used for new systems as well as for replacement parts, and the FTS calorimetric flow switch has recently completed successful tests in the Reasearch and Development centre.

Jason Atkinson, Head of Technical and Product Development stresses that, while performance of the technology is important, it’s supply chain relationships that are mission critical. “From the customers’ point of view, it’s the Byworth Boiler that performs, not any one of the instruments or control systems on it. So, our suppliers need to be long-term partners. We got solid reliability from SICK from the beginning. They have adapted their technology, provided training and support for us and our customers, and they have grown to understand our process very well.”

 

 

Wide range of fluid sensors from SICK
Wide range of fluid sensors from SICK
Wide range of fluid sensors from SICK
Wide range of fluid sensors from SICK

 

Standardization of instrumentation

Standardization of instrumentation has been a continuing journey across the entire Byworth boiler range, explains Atkinson. This not only benefits customers, but also optimises the company’s own operational efficiency.

“The boiler industry is quite a conservative industry, so sometimes we have to push a little to recommend using the best technologies. We have driven out traditional boiler instrument suppliers to put SICK sensors on our equipment. We use SICK’s PBS pressure sensors to control the hot well tank level, as well as to regulate steam pressure output from the boiler. The PBS is a transmitter with two switch points. So, instead of having 3 or 4 different instruments, we could use one instrument on two different boiler designs. This also helped us move away from 230V and 110V towards a standard 24V DC control architecture. Not only does this save energy, space and reduce wiring, but the PBS pressure transmitters from SICK are all on M12 plug connectors, which makes it easier for our service engineers. They are just plug and play.”

The PBS’s on-sensor display enabled Byworth to reposition the pressure reading on the hot water feed, from the top of the tank to a workable, eye-level height. For many customers, the PBS’s added analogue output has also proved an advantage, and again reduced the need to install another separate sensor.

 

We use SICK’s PBS pressure sensors to control the hot well tank level, as well as to regulate steam pressure output from the boiler.
SICK’s PBS pressure sensors
We use SICK’s PBS pressure sensors to control the hot well tank level, as well as to regulate steam pressure output from the boiler.
SICK’s PBS pressure sensors

 

Guided wave radar technology for sensing water level in the boiler

Perhaps the greatest technology step-change of all came when SICK introduced a new guided wave radar technology, which Atkinson recognised could be used for sensing water level in the boiler. Until the arrival of SICK’s LFP Inox sensor, Byworth had used either a capacitive sensor or a float system for continuous level measurement of water in the boiler. The capacitive sensor technology proved to be sensitive to foam and the float system sensitive to turbulence in the boiler.

The LFP Inox from SICK overcame both of these challenges as it is neither sensitive to water foaming when being poured into the boiler or turbulence.

“The LFP guided wave radar gives us a much more reliable, accurate level, so we can run our feedwater system much more tightly,” says Atkinson. “We do not get so many swings in water level. The more the water level fluctuates, the less heat efficient the system is.” SICK was able to develop a firmware adaptation for the LFP to meet the combined requirements of a sensor insensitive to foam and turbulence with a display that is easily accessible to a boiler operator or service engineer. Not only did this mean the Byworth LFPs could be standardized on a 1.3 metre probe length, but the LFP’s amplifier system offered a solution to separating probe and electronics to give operators easier access to the display. So, the LFP in-tank probe is connected remotely to the sensor and emitter via a flexible coaxial cable which can be up to 3.3 metres long.

 

 

Successful trials with DOSIC ultrasonic flow sensor confirm competitiveness and accuracy
Level sensors LFP Inox
Successful trials with DOSIC ultrasonic flow sensor confirm competitiveness and accuracy
Level sensors LFP Inox

 

Successful trials with DOSIC ultrasonic flow sensor confirm competitiveness and accuracy

Byworth’s successful trials of the DOSIC ultrasonic flow sensor from SICK confirmed its competitiveness and accuracy, so it has been introduced for feed tank metering on the smaller boiler range. Because feedwater has often undergone a reverse osmosis process, it can have a very low conductivity, so a magnetic flow meter could not be used. The DOSIC has also proved useful for fuel oil metering. Meanwhile, trials have recently completed to use SICK’s new calorimetric FTS thermal flow switch to monitor flow in the softener drains. Standardizing and rationalising into one central control was the concept behind Byworth’s ground-breaking Unity digital control system, which won a Queen’s Award for Enterprise in Innovation in 2016. Traditionally boilers have evolved with individual control systems for different parts of the boiler.

“On the Unity systems we have done studies that demonstrate fuel savings of 7 per cent annually, over and above what is achieved just by installing new plant. That’s based around how we control everything from one unit in the boiler house, rather than in separate, individual processes - how we sequence boilers, how we modulate them, how we bring them online and so on,” says Atkinson. “Standardizing on sensors helps us to control the data coming from different parts of the boiler house a lot more finely. Of course, we are looking for accuracy, reliability and repeatability of measurement, too. Instruments like the guided wave radar were a hard sell for us to begin with, and we had to explain our rationale for using suppliers not traditionally associated with the boiler industry. But now those technologies are being asked for by customers and specified for new boilers. We have had to drive that change through.

“Our relationship with SICK has been a mutually beneficial partnership, where both companies have ended up with a better product.”

 

 

 

Read more:

Ultrasonic flow measurement for steam: the smart choice

Smart Fluid Power: Easy integration in hydraulic and pneumatic systems

DOSIC - compact stainless-steel sensor for flexible flow measurement

Level and temperature monitoring in transformer stations

 

 

Xaver Meier

Head of Business Unit Industrial Instrumentation

Xaver Meier has led the Product Management and Applications Engineering Departments, focusing on Industrial Instrumentation, since early 2015.