How the cement industry, refineries and chemical factories reduce their carbon emissions

17.6.2024

The production of cement for the construction industry is responsible for approx. 7% of all man-made CO2 emissions. It is therefore essential that the cement industry in particular reduce its CO2 emissions. Enormous quantities of CO2 are also produced, however, when producing ammonia for refineries and chemical factories. But how can these industries reduce their environmental footprint, and what sensor solutions does SICK offer?

Welcome to part seven of our series on decarbonization where we focus on the cement and chemical industry.

The chemical and cement industries cause high CO2 emissions.
The chemical and cement industries cause high CO2 emissions.

Decarbonization of the cement industry

The SCPS3300 gas analysis system enables quality control and process optimization.

 

 

Globally, the cement industry contributes to 7% of CO2 emissions. Around two thirds of these emissions can be attributed to raw material related processes. A further third result from energy-related CO2 emissions through the use of fuels.

Faced with this challenge, the industry has set itself the ambitious goal of decarbonizing its energy and resource intensive processes over the coming years. Various technologies are available for this: improving the thermal efficiency, reducing the clinker content in cement, greater use of alternative fuels and renewable energy sources, and using CCUS technologies.

SICK assists cement producers along the entire value adding chain with reducing their emissions and optimizing processes. The SCPS3300 gas analysis system, for example, is used for quality control and process optimization.

Continuous emission monitoring systems such as the MCS200HW are used to monitor emissions.

In addition to a comprehensive portfolio of products for measuring gases, dust, and flow, SICK focuses in particular on the automation and digitalization of existing processes to adapt them to the new requirements. With its broad range of hardware, software and service solutions, SICK is a competent partner for the cement industry in jointly achieving and realizing the goals it has set itself.

SICK offers various products for measuring gases, dust and flow.
SICK offers various products for measuring gases, dust and flow.
Kaasuanalysaattorit

Decarbonization in chemicals, petrochemicals, and refineries

Since ammonia will also be used in future as a carbon-free fuel, reducing the carbon intensity in the production of ammonia is an important goal.

The “blue” ammonia production process uses the same hydrocarbon raw materials except with a carbon capture system for isolating and removing the CO2.

In “green” ammonia production, hydrogen is obtained through the electrolysis of water and nitrogen. The energy for driving these plants is generated from renewable energy sources such as solar and wind energy.

Burning ammonia in air produces nitrogen oxides which, when dissolved in water, form nitric acid - an important base chemical for fertilizer production. Several residual nitrogen oxides remain in the exhaust gas, however, along with nitrous oxide (N2O), an important greenhouse gas that is produced as a by-product in the combustion process. Waste gas reduction technologies are used to reduce the NOx and N2O concentrations. MCS200HW CEMS solutions control the DeNOx reduction units and report the emissions.

Exhaust gas reduction technologies are used to reduce NOx and N2O concentrations.
Exhaust gas reduction technologies are used to reduce NOx and N2O concentrations.

 

Read the other parts of our series on decarbonization

Low-carbon combustion and production processes

Read more in part one of our series on decarbonization

Decarbonization: gas analysis and flow measurement for transfer and process applications

Read more in part two of our series on decarbonization

Decarbonization in the energy sector

Read more in part three of our series on decarbonization

Decarbonization in shipping and air transport

Read more in part four of our series on decarbonization

Decarbonization approaches in mining and metal production

Read more in part five of our series on decarbonization

Reduction of greenhouse gases in the waste management industry

Read more in part six of our series on decarbonization

 

The products
featured in this
article are now
supplied by Endress+Hauser.

Click here for the products on endress.com