EN
Country: EN (China)
Select country/region

Language

  • English
  • Chinese
web-tension-control-stage-teaser-component-image

Monitoring the web tension

Trouble-free processes thanks to sensor solutions from SICK
Get in touch with us!

Ensuring the correct tension

In the packaging or textile industry, the uniform web tension of the material to be processed is crucial for a trouble-free process flow. A too low tension, for example, can result in the material not being guided properly. If the tension is too high, the material is stretched, which in turn can distort processes such as printing and cutting or even cause the material to tear. This results in unplanned downtimes and falling productivity. Sensors from SICK help prevent defects, monitor product quality, and maintain production flow.

SICK offers position sensors and linear encoders for monitoring the web tension

MONITORING WEB TENSION USING WITH POSITION SENSORS

Ensuring the correct web tension when using pneumatic cylinders

A so-called dancer is used to compensate for irregularities when unwinding the web material and to establish a constant web tension for the feeding process. To do this, the dancer position is regulated to the center position. Deviations from this are detected by the position sensor mounted directly on the pneumatic cylinder. When tensioned correctly, the web material runs precisely and defects, such as those caused by inaccurate sealing of tubular bags, do not occur.

Sensor measures web tension in a pneumatic cylinder

MONITORING WEB TENSION USING LINEAR ENCODERS

Ensuring the correct web tension when using hydraulic cylinders

The dancer is used to compensate for irregularities when unwinding the web material. To do this, the dancer position is regulated to the center position. The linear encoder is suitable for determining the absolute position of piston rods in hydraulic cylinders and reliably detects possible deviations. This ensures that the correct tension is always applied. Further intelligent functions for condition monitoring, for example, allow predictive maintenance and create transparency about the current machine condition. This minimizes unplanned downtimes and increases the efficiency.

Sensor measures web tension in a hydraulic cylinder