EN
Country: EN (China)
Select country/region

Language

  • English
  • Chinese
SM_MA_~1.JPG

Mobile applications

Adaptive safe movements

Easily solve applications with mobile robots

Mobile robots and AGVs should be fast but not endanger the personnel, transported goods, or vehicle surroundings on their routes. It must therefore be continuously ensured that these vehicles take evasive action or stop if necessary.

Automated guided vehicles drive autonomously through an industrial hall

Safely on the move

High mobility is a basic requirement for the effective and flexible use of mobile robots. To keep them moving, Safe Motion solutions monitor vehicle speeds and steering angles and adjust them individually for different driving situations. A balanced design of the driving motion leads to high productivity and ensures the safe and efficient use of your vehicle fleet.

Two arrows collide and cause a collision

Collision avoidance

Vehicles have to detect hazards within the braking range during operation. The protective fields of a safety laser scanner ensure the safety of people and objects when AGVs and mobile robots are in use. A safety controller adjusts these protective fields in relation to the speed and steering angle of a vehicle. When driving around curves, a safely reduced speed prevents the vehicle from tipping over or losing its load.

Arrow on circle shows the speed of a movement

Safe movement monitoring

Safe movement monitoring is the prerequisite for free navigation of AGVs and mobile robots in factories and warehouses. That is why safety encoders and safe motor feedback systems reliably record the speed and steering angles of these vehicles. Safety controllers and Motion Monitoring modules evaluate the respective data to avoid collisions of vehicles with people and objects.

The hand indicates a hazardous situation and prompts a person to stop

Safe stopping

When combined with a safety controller, the protective fields of a safety laser scanner also enable an autonomous vehicle to avoid obstacles and stop if necessary. If, for example, a person interrupts a protective field, the safety controller safely monitors the braking ramp and, if necessary, initiates an emergency stop of the vehicle.

EFFICIENT DRIVING

Vehicles move about freely in a hall based on the collected data

Use rooms efficiently

Safe Motion makes safe drive and motion monitoring of AGVs and mobile robots possible. These are equipped, among other things, with DFS60S Pro safety encoders that record data on the direction and speed of travel.
The Flexi Soft Drive Monitor uses this information to monitor adherence to the direction and speed parameters of the vehicles. They are also equipped with safety laser scanners whose protective fields protect the vehicles and their surroundings.
The protective fields of the attached safety laser scanners are activated for this purpose. This reduces the space required for driving movements and ensures a high vehicle availability.

An automated guided vehicle fetches the load

MAKING AUTONOMOUS DRIVING SAFE

Human and automated guided vehicle stay together in an industrial hall

Tailored driving processes

The DFS60S Pro safety encoders on the drive axles of an AGV provide information about vehicle speed and steering angle. These data provide the foundation for implementing the safely limited speed (SLS) and safe speed monitoring (SSM) as well as safe direction (SDI) safety functions. These functions ensure, among other things, that the speed of an AGV automatically adjusts to the particular load and routes. A vehicle will drive slower, for example, in curves. Individual and independent driving profiles can be designed.

An automated guided vehicle system with a full load

SAFE MOTION AND EFI-PRO

Multiple workstations are connected and work together

EFI-pro for advanced capabilities

The EFI-pro communication interface ensures an even more efficient interaction between the safety controller and safety sensors in Safe Motion applications. This significantly increases the number of definable monitoring cases. Vehicle information such as speed, steering angle, and load condition can be used, for example, to switch the protective fields of safety laser scanners in even smaller increments and with greater precision. This helps you avoid unplanned downtimes and increase the productivity of your vehicles.

A cleaning robot at work in an industrial hall

FLEXIBLE PROCESS CONTROL

Car drives out of a production line

Safe movement monitoring optimizes process flows

Safe Motion solutions make it possible to monitor the directions of movement and stopping processes of machine parts and automated guided vehicle systems. In the automotive industry, for example, Safe Motion helps mobile robots move about freely in factories and warehouses. This allows you to optimize processes down to batch size 1, since the mobile robot only approaches relevant assembly stations.

The body of a car and the engine are assembled

MOBILE OUTDOOR APPLICATIONS

Automated guided vehicle system travels outdoors

Safe movements beyond the hall limits

Increasing passenger numbers and rising cost pressures necessitate a higher level of automation at airports, e.g., through automated docking and undocking of passenger boarding bridges. Safe Motion solutions combining the Flexi Soft safety controller, Flexi Soft Drive Monitor, and outdoorScan3 safety laser scanner are ideal for this purpose. The safety controller switches the protective field of the safety laser scanner depending on the steering angle of the passenger boarding bridge. Safe steering angle detection is performed in the motion monitoring module. If the protective field is interrupted, the Safe Motion solution stops the mobile robot and thereby protects people.

A passenger boarding bridge docks with an aircraft