Automated quality assurance for the mobility of tomorrow
Learn more
Home Industries Industries Sensor solutions for the automotive industry Sensor solutions for vehicle manufacturing
Vehicle manufacturing is undergoing a transformation: electromobility and digitalization are shaping industrial automation along the entire value-adding chain – from the body shop to the paint shop. At the same time, expectations of flexibility, efficiency and sustainability in automotive manufacturing are growing. Topics such as process reliability, traceability and quality-assured inline testing/ inline quality assurance are coming more into focus and are crucial for modern automotive automation. As a longstanding partner, SICK knows the requirements of the industry inside out and provides future-proof complete solutions comprising hardware, digital products and services that support end-to-end production processes, enable traceability and reliably safeguard productivity. SICK thereby creates the basis for efficient and sustainable quality assurance in the automotive industry.
Sustainability in the automotive industry means reducing the environmental impact over the entire life cycle of a vehicle – from the extraction of raw materials to production, use and recycling. This includes measures such as CO₂ reduction, energy-efficient production, the use of recyclable and sustainable materials and the promotion of clean drive systems such as electric and hybrid vehicles.
Stricter emission and reporting requirements also play a central role, obliging manufacturers to use more climate-friendly and resource-saving processes.
Inline quality assurance in vehicle manufacturing means that quality checks are carried out directly during the production process. Sensors, cameras, lasers or ultrasound record parts in real time, detect deviations immediately and enable automatic corrections in the process. Modern, AI-supported image processing identifies surface defects, dimensional deviations or incorrectly assembled components early – without interrupting the production flow. The result: less waste and rework as well as greater efficiency, process stability and traceability.
Vehicle connectivity refers to the ability of a vehicle to continuously exchange data with its surroundings, digital services and other road users. This includes connections to other vehicles (V2V), to the infrastructure (V2I), to the cloud (V2C) and comprehensive V2X communication that combines all channels. Modern connectivity is based on technologies such as IoT, 5G and cloud services and enables functions such as real-time navigation, remote diagnostics, over-the-air updates, safety assistance systems and personalized services in the vehicle.
Decarbonization in the automotive industry means reducing CO₂ emissions along the entire value-adding chain – from material extraction and vehicle production to use and recycling. This includes measures such as the expansion of electric and hybrid vehicles, the use of sustainable materials, greater energy efficiency in production and the switch to renewable energies in production and supply chains.