Safety laser scanners are powerful devices for complex applications. With a vast number of choices in the market with regards to range, connectivity, size, and robustness, there are many variables to consider when designing a safety solution using scanners. Based on the experience of Martin Kidman, Product Specialist Machinery Safety from SICK (UK) Ltd., here are six examples and common mistakes made when setting up safety laser scanners.
Six common mistakes when setting up safety laser scanners
1. Installation and mounting: thinking about safety last
If you are going to remember just one point, then this is it! Too many times have I been present at an "almost finished" machine and asked, "Right, where can I stick this scanner?". Inevitably, what ends up happening is that blind spots (shadows created by obstacles) become apparent all over the place. This necessitates mechanical "bodges" and maybe even additional scanners to cover the complete area when one scanner may have been sufficient if the cell had been designed properly in the first place. In safety, designing something out is by far the most cost-effective and robust solution. If you know you are going to be using a safety laser scanner, then design it in from the beginning; this could save you a world of pain. Consider blind zones, coverage and the location of hazards. This also goes for automated guided vehicles/carts. For example, the most appropriate position to completely cover an AGV/AGC is to have two scanners adjacent to each other on the corners integrated into the vehicle.
2. Configuring incorrect multiple sampling values
An often misunderstood concept – multiple sampling – indicates how often an object has to be scanned in succession before a safety laser scanner reacts. By default and out of the box, this value is usually x2 scans, which is the minimum value. However, this value may vary from manufacturer to manufacturer. A higher multiple sampling value reduces the possibility that insects, weld sparks, weather (for outdoor scanners) or other particles cause the machine to shut down. Increasing the multiple sampling can make it possible to extend a machine's availability, but it can also have negative effects on the application. Increasing the number of samples is basically adding an OFF-Delay to the system, meaning that your protective field may need to be bigger due to the increase in the total response time. If a scanner has a robust detection algorithm, you shouldn't have to increase this value too much, but when this value is changed you could be creating a hazard due to lack of effectiveness of the protective device. If it is changed, you should make a note of the safety laser scanner's new response time and adjust the minimum distance from the hazardous point accordingly to ensure it remains safe. Furthermore, in vertical applications, if the multiple sampling is set too high then it may be possible for a person to pass through the protective field without being detected, so care must be taken! For one of our latest safety laser scanners – the microScan3 – we provide the following advice:
| Recommended multiple | Application |
| 2x | Stationary application: such as horizontal hazardous area protection or vertical hazardous point protection under clean ambient conditions |
| 2x | Stationary application: such as vertical access protection (only 2-time multiple sampling may be used for vertical access protection) |
| 4x | Mobile applications |
| 8x | Stationary application: such as horizontal hazardous area protection under dusty ambient conditions |
3. Incorrect choice of safety laser scanner
The maximum protective field that a scanner can facilitate is an important feature, but this value alone should not be a deciding factor as to whether or not the scanner is suitable for an application. A safety laser scanner is a Type 3 device according to IEC 61496 and an Active Opto-Electric Protective Devices responsive to Diffuse Reflection (AOPDDR). This means that it depends on diffuse reflections off objects. Therefore, to achieve longer ranges, scanners must be more sensitive. In reality, this means that sometimes scanning angle, but certainly detection robustness, can be sacrificed. This could lead to a requirement for an increasing number of multiple samples and maybe a lack of angular resolution. The increased response times and lack of angle could mean that larger protective fields are required and potentially even additional scanners; despite having purchased a longer range device! A protective field should be as large as required but as small as possible. A shorter range scanner may be more robust than its longer range big brother and hence keep the response time down, reduce the footprint, lower cost and eliminate annoying false trips.
4. Incorrect resolution selected
The harmonized standard EN ISO 13855 can be used for the positioning of safeguards with respect to the approach speeds of the human body. Persons or parts of the body to be protected may not be recognized or not recognized in time if the positioning/configuration is incorrect. The safety laser scanner should be mounted so that crawling beneath, climbing over and standing behind the protective fields is not possible. If crawling under could create a hazardous situation, the safety laser scanner should not be mounted any higher than 300 mm. At this height, a resolution of up 70 mm can be selected to ensure that it is possible to detect a human leg. However, it is sometimes not possible to mount the safety laser scanner at this height. If mounted below 300 mm, a resolution of 50 mm should be used. It is a very common mistake to mount the scanner lower than 300 mm and leave the resolution on 70 mm. Reducing the resolution may also reduce the maximum protective field possible on a safety laser scanner, so it is important to check.
5. Ambient/environmental conditions not considered
Sometimes safety laser scanners just aren't suitable in an application. And coming from someone who sells and supports these devices, that is a difficult thing to say! However, scanners are electrosensitive protective equipment and infrared light can be a tricky thing to work with. Scanners have become very robust devices over the last decade with increasingly complex detection techniques (safeHDDM® by SICK) and there are even safety laser scanners certified to work outdoors (outdoorScan3 by SICK). However, there is a big difference between SAFETY and AVAILABILITY, and expectations need to be realistic right from the beginning. A scanner "might" not maintain 100% machine availability if there is heavy dust, thick steam, excessive wood chippings, or even dandelion seeds etc. constantly in front of the field of view. Even though the scanner will continue to be safe and react to such situations, trips due to ambient conditions may not be acceptable to a user. For extreme environments, the following question should be asked: "What happens when the scanner is not available due to extreme conditions?" which can be especially true in outdoor application in heavy rain, snow or fog. A full assessment of the ambient conditions and potentially even proof tests should be carried out. This particular issue can become a very difficult (sometimes impossible) and expensive thing to fix.
6. Non-safe switching of field sets
A field set in a safety laser scanner can consist of multiple different field types. For example, a field set could consist of four safe protection fields (field set 1) or it could consist of one safe protective field, two non-safe warning fields and a safe detection field (field set 2).
Martin Kidman
Product Specialist Machinery Safety SICK (UK) Ltd.
Martin Kidman gained his Ph.D. at the University of Liverpool in 2010 and has been involved in Industrial Automation since 2006 working for various manufacturers of sensors. He has been at SICK UK Ltd. since 2013 as a product specialist for machinery safety providing services, support and consultancy for industrial safety applications. He is also a certified Functional Safety Engineer (TUV Rheinland, #13017/16).