You searched for "flowsic"

194 results:

Result 1 - 24 out of 194

  • Cutting-edge technology: ultrasound
  • Diagnostics and permanent operational check
  • Rugged and reliable due to lack of moving parts
  • Exchangeable cartridge
  • Straight inlet/outlet zone not required
  • Overload-proof
  • Optional integrated flow conversion / date registration
  • Battery or intrinsically safe power supply
Compare now
Select
  • Measurement availability under all operating conditions, at high gas velocities and with changing gas compositions
  • Intuitive FLOWgateTM operating software
  • I-diagnosticsTM for self-monitoring, easy verification and condition-based maintenance of the system
  • Retrofit solutions for existing measurement systems
Compare now
Select
  • User-friendly product family
  • Automatic correction of pressure and temperature effects
  • Available for all operating conditions
  • PowerIn Technology™ for reliable backup operation
  • Intelligent application diagnostics with i-diagnostics™
  • Extendable with flow computers per connect-and-go
Compare now
Select
  • Rugged titanium converters for long service life
  • Corrosion-resistant material for use with aggressive gases (option)
  • Integrated measurement via duct diameter for types H, M, and S
  • Probe version PR for cost-saving, single-sided installation in duct
  • Automated operational check with zero and reference point test
Compare now
Select
Small, but a global leader all the same: Ehrler Prüftechnik Engineering GmbH (EP-E) has crafted a remarkable reputation in the field of high-precision testing and calibration systems. A preferred... Read on
A climate-friendly and promising application is emerging for the natural gas network. Operators of gas grids can keep up with the trend to feed, transport and store regeneratively produced hydrogen in... Read on
The new  FLOWgate™ operating software for all FLOWSIC ultrasonic gas flow meters and ultrasonic gas flow measuring devices from SICK links diagnostic data quickly and intelligently and presents... Read on
Green technologies for producing energy are creating real hope: Bio-coal can already be produced synthetically through CO2 recycling, bio-butanol can be made with genetically- modified microbes and bio-gas... Read on
Depending on the system capacity and location, solar power plants can supply entire regions with environmentally-friendly energy all day long. Operating entities are not happy until systems are working... Read on
 FLOWSIC600-XT - the new gas flow meter from SICK seamlessly preserves its predecessors positive image as an outstanding precision measurement device for demanding industrial environments. The FLOWSIC600-XT... Read on
Many industries are successfully employing SICK's ultrasonic technology for flow and volume measurement in natural gas pipelines, industrial plants, and exhaust ducts. But is ultrasound also the best technology... Read on
Now there is no need to go without ultrasonic precision and fall back on other mechanical measurement techniques in the event of a mains voltage failure. The back-up batteries in the FLOWSIC-X gas flow... Read on
HOUSTON, TEXAS, AUGUST 24, 2021 – In strategic partnership with Eagle Research Corporation (ERC), SICK is launching an exciting new addition to enhance the FLOWSIC500 flow meter device.ERC is an... Read on
South Africas largest electricity producer ESKOM has set itself a significant task: to continuously monitor its dust concentration levels and, at the same time, meet the requirements stipulated by the... Read on
When it comes to achieving climate protection objectives or making fundamental improvements to our operational performance, there are many aspects to analyze and evaluate. The approaches to this are particularly... Read on
  • Quality components
  • Modular flexible installation
  • Non-contact ultrasonic technology without pressure loss
  • Measuring range span greater than 100 : 1
  • Sensors can be replaced under pressure
  • Low sensitivity to pulsation and pressure regulator noise
  • Remote electronics (max. 15 m)
  • Bi-directional measurement with automated diagnostics
Compare now
Select
  • Highly efficient ultrasonic transducer - up to gas temperatures of 280 °C and pressures up to 450 bar
  • Direct path layout
  • Intelligent self-diagnostics
  • Compact, robust design
  • Integrated log book and data logger
  • Large measuring range 1:120
  • Bidirectional measurement
  • Low power consumption: <1 W
Compare now
Select
  • Real-time ultrasonic exhaust gas flow measurement
  • Independent from pressure, temperature and gas composition
  • Outstanding measurement accuracy
  • For exhaust gas temperatures up to 600 °C
  • Direct measurement made in undiluted exhaust gas
  • Heated measuring section
  • Minimum backpressure
  • Small footprint, mobile, flexible process connections
Compare now
Select
  • Very large measuring distances possible
  • Non-contact measurement
  • Extremely rugged components made of titanium, stainless steel, or die cast
  • Versions for very corrosive tunnel atmospheres
  • Determination of flow direction
  • No mechanical moving parts
Compare now
Select
  • High-resolution measurement and short response time
  • Innovative sensor design for very high gas velocities and gas temperatures up to 280 °C
  • Optimal signal transmission even under atmospheric pressure
  • Detached installation of the control unit up to 1,000 m away
  • Single and multi-path configuration, opt. Probe version
  • Zero point test in the field according to factory standard
  • Control cycle for automatic self-diagnosis / signal optimization
Compare now
Select
  • High turndown ratio
  • Designed for wet gas applications
  • Intelligent meter diagnostics incl. wet-gas detection
  • Possibility for remote monitoring thanks to digital interfaces
  • Two-wire-transmitter with digital HART® interface
  • Full integration of pressure- and temperature measurement, volume conversion and energy flow rate calculation
Compare now
Select
The demand for cleaner air emitted from cars is increasingly determining the exact test technology required and the associated growing requirements on measurement technology. The ultrasonic technology... Read on
In the Netherlands, natural gas is a key source of energy and accounts for nearly half of the total energy mix. As we enter a new era in terms of energy, an intelligent approach to gas production is crucial... Read on
Every day natural gas flows in great quantities through pipelines or into storage facilities. Precise gas quantity measurement is of the utmost importance, as even very small measurement errors could result... Read on

Result 1 - 24 out of 194