You searched for "flowcomputer"

52 results:

Result 1 - 24 out of 52

Newer-generation flow computers combine functionality with user-friendliness. They are the preferred device for use in custody transfer gas measurement, are approved according to the EU's Measurement Instruments Directive, and comply with the relevant international standards. The easy integration of temperature, pressure, and flow measurement values via digital and serial interfaces is used to convert recorded volumes. The flow computers use industry-standard conversion algorithms.

Ultrasonic technology is particularly attractive for custody transfer flow measurements when it comes to invoicing for gas levels, and also for measuring flare gas. With its individual components... Read on
Today, Australia is the second largest exporter for LNG in the world with high growth rates in gas production. The Roma gas field was one of the first discovered fields in Australia. The field covers approximately... Read on
Natural gas is a fundamental resource which plays a crucial role within Italian energy systems. It is for this reason that the modernization of the installations and infrastructures dedicated to its transport... Read on
Over half of the around 80 biomethane plants in the UK measure the gas volume upstream of the infeed using FLOWSIC500 units from SICK. British system integrator Thyson in particular values the trouble-free... Read on

Type: Operating instructions

Part number: 8015675

Title: Flow-X Gas flow computer

Release date: Dec 1, 2021

Size: 6.11 MB

Download
Every day natural gas flows in great quantities through pipelines or into storage facilities. Precise gas quantity measurement is of the utmost importance, as even very small measurement errors could result... Read on

Type: Product information

Part number: 8017524

Title: Flow-X Flow computers

Release date: Feb 1, 2019

Size: 767.00 KB

Download
  • Complete calibration is possible
  • Customization of instrumentation including gas analyzer, gas chromatograph, and supervisory computer
  • Seamless integration with the flow computer Flow-X from SICK
  • Available from Class 150 to Class 2500
  • Modular design
Compare now
Select
RoviMo® is the world’s first fully electric, CO2 emissions free autonomous multi-purpose robot for large green spaces. The idea for an autonomous robot vehicle for maintaining sports fields,... Read on
With the construction of the most advanced car tower in Switzerland, the Züri West car dealership in Schlieren can now offer its customers a very special shopping experience. At the press of a button,... Read on
SICK has more than 30 years’ experience in the field of vision technology. This expertise is exploited in the continuous development of innovative and intelligent solutions for identification, positioning,... Read on
Executive and Supervisory Board members of SICK AG
SICK has been developing sensors for over 75 years. During that time the company has always been a little bit ahead of the times. We spoke to Christoph Müller, Senior Vice President for Industrial... Read on
Protecting your privacy is important to us and we want you to feel secure while visiting our website.
Velux is renowned for high-quality windows and the accessories that go along with them. Dedicated to always finding the best solution, the software department developed software that the company uses to... Read on
The increasing individualization of products turns single units into a production batch that will be in demand with growing frequency in future. Production processes will have to be converted to cope with... Read on
DS Smith, a worldwide leading provider of sustainable packaging solutions, paper products and recycling services, needed to upgrade an end-of-line monitoring solution to automate a labor-intensive process,... Read on
  • Utilises the ultrasonic flow meters FLOWSIC600 or FLOWSIC600-XT
  • Available from DN 50 to DN 1200 from Class 150 to Class 2500
  • With calibration the uncertainty of 0.1% is achievable
  • Customization of system components
  • Seamless integration with the SICK Flow-X flow computer
Compare now
Select
Increasing product type diversity, more frequent model changeovers, quantity fluctuations: The changing market conditions call for suitable and competitive product solutions, for example precise 3D measurements... Read on
In 2015, the young Danish company Mobile Industrial Robots (MiR) introduced the German market to the MiR100, a mobile transport robot that works like clockwork. Built-in S300 safety laser scanners, 3D... Read on
Protecting your privacy is important to us and we want you to feel secure while visiting our website.
Whether its the Watchman, Optotrap OTD or PLS - SICK represents innovation in laser scanner development. SICK has been working in the field of laser scanners for nearly 40 years and recognized early that... Read on

Result 1 - 24 out of 52