EN
Country: EN (United States)
Select country/region

Language

  • English
stage-teaser-image-component-reute

Reute

One site, plenty of possibilities.
All jobs in Reute

Reute is SICK AG's second-largest site after the headquarters in Waldkirch. Among other things, e-card production and rapid prototyping are located here. 

In addition, the Logistic Technology Center, where SICK sensors are tested under real conditions, is located in an area of 1,000 m² in Reute.

Exterior view of the SICK location in Reute

Reute - In the bay of Breisgau

Reute lies in the middle of the Rhine plain between the Kaiserstuhl and the Black Forest, with the Glotter river flowing through it at the southern edge of the village.

Reute from above