Edge guiding
The optical paper edge detection system is capable of regulating a web with an accuracy of approximately 50 μm. The AT20 array sensor works according to the scanning principle and therefore does not require a reflector. Mounted above the paper web, it is not susceptible to contamination. For sophisticated applications (transparent films, for example), it is also possible to use the AL20 array sensor with a reflector.