EN
Country: EN (United States)
Select country/region

Language

  • English
industry-drives-controls-header-image-03-webx
industry-drives-controls-applications-01-image-webx
Machines and materials

Sensor solutions for automation and motion control

Safe drive solutions and flexible automation using intelligent sensor technology - The future in motion!
Learn more

The right solution for your application

FAQ

The position monitoring of a pneumatic cylinder is important for reliable process control in automation engineering. As the metal housing does not allow a view of the piston, various physical measuring principles are used to detect whether the piston is retracted or extended or has reached a defined intermediate position. The most common method is the use of magnetic cylinder switches. The piston contains a permanent magnet. Corresponding sensors are mounted on the outside of the cylinder barrel – usually in a slot. When the magnet passes the sensor, it switches and reports the respective piston position.

A Motion Control system controls movements in machines with high-precision by precisely regulating the position, speed and acceleration of a load. It typically consists of a drive system, sensors, drive and controller, which together enable precise, repeatable and efficient motion sequences – a central component of modern automation.

In industrial drive technology, the terms encoder and motor feedback system are often used interchangeably. From a technical point of view, however, a motor feedback system is a specialized further development of the classic encoder. An encoder is a basic sensor that converts mechanical movements – rotations or linear displacements – into electrical signals. It provides precise information on position, speed and direction of rotation. A motor feedback system is an advanced, intelligent encoder that is integrated directly into the control circuit of a servo motor. It communicates specifically with the servo controller (inverter) and enables particularly precise and dynamic motor control.

Industrial drive technology includes systems such as motors, gearboxes, drive controllers and sensors that generate and control movements in machines. It ensures that systems work precisely, efficiently and reliably – whether in conveyors, packaging, robotics or machine tools.

A basic distinction is made between direct measuring systems (integrated in the cylinder) and indirect measuring systems (externally mounted). Direct measuring systems are installed in the cylinder and are therefore optimally protected against dirt, shocks and external influences. Magnetostrictive displacement transducers are used here – the industry standard for precise position measurement. A waveguide is located in a bore in the piston rod. A position magnet on the piston generates a mechanical pulse whose runtime is measured. Advantages: non-contact, wear-free, very high measurement accuracy.