Cleanrooms in semiconductor manufacturing are clearly their domain: robots are the order of the day here in all their various guises. Track-guided, stationary or mobile, they assist with production and loading/unloading. Mobile robots are gaining importance in this area. In contrast to tracked guided systems, they are more flexible and can move around freely within the room. For the specialists at Fabmatics, mobile robots have already become an integral part of any intelligent robotics solution for transporting wafers – the silicon discs on which microchips are produced. In the case of the freely moving HERO®FAB, the safety laser scanners and photoelectric sensors from SICK play a decisive role in particular in the area of safety and the positioning of the gripper. While not always evident at first glance, they are the hidden “Heroes of safety” in the HERO®FAB.
No half-measures – Fabmatics and SICK are making mobile robots safe
Specialists in semiconductor production
Fabmatics GmbH in Dresden develops intelligent automation and robotics solutions for customers in the semiconductor industry. The company has a unique expertise in supplying complex automation, robotics and handling systems for use in cleanroom conditions. A task with a great deal of responsibility: “Our various robots are, after all, transporting very valuable goods within the semiconductor production environment. It is therefore par for the course that each single one of our robots carries the value of a single family home ‘on its shoulders’”, says Martin Däumler, Group Manager Product Development & System Integration at Fabmatics. That makes it all the more important to find reliable solutions. The prerequisites for safe mobility can be fulfilled, amongst other things, with the help of partners like SICK who can offer both hardware as well as software, planning and development, manufacture and installation right through to after sales service from a single source. In this application, the S300 Expert safety laser scanner, and in future the microScan3, take care of tasks relating to horizontal and vertical protection within the room. The miniature photoelectric sensors from the W2S-2 family create an intelligent sensor solution for loading and unloading by the grippers – small, smart and light.
Mobile in the cleanroom
The HERO®FAB brings mobility to the cleanroom. It combines an established, clean and safe robot system with an innovative automated guided vehicle platform. It was developed to fully automatically load and unload production equipment and to enable items to be quickly transported between individual process steps and also intermediate storage areas within the cleanroom. Specifically, it can move up to four containers at a time – in cleanrooms, these containers are typically used to transport 25 individual 200mm or 300mm wafers. Special versions of the HERO®FAB with a large 60l water basin are also used. Based on the earlier tried-and-proven HERO®Rail rail solution, the further development of the HERO®FAB now makes it possible to move around freely within the cleanroom without a rail or cable connection. Thanks to the safety laser scanners from SICK, the mobile robot not only fulfills the object safety requirements, but also the most demanding safety requirements for the interaction of humans and machines within the same working space. Various levels of personal safety can be guaranteed depending on the degree of interaction and the local requirements.
Perfect for small installation spaces
The miniature photoelectric sensors in the W2S-2 family guide the robot arm safely and reliably when gripping the valuable items. The particularly useful aspect is also their size. Installation spaces can often be very tight, in particular in mobile robots. The controller already takes up about 80% of the available space inside the robot. That is another reason why the W2S-2 was chosen. The ultraflat G2 flat sensors can be integrated into miniature systems and very tight installation spaces. They are also characterized by their outstanding detection thanks to a high-performance background suppression feature. Even very small objects can be detected without difficulty starting at distances of just 8 mm. Jet black, reflective, transparent and shiny objects can also be reliably detected.
Tried-and-proven interfaces for the future
Ease of installation is another advantage when integrating a safety controller into the mobile robot. The safe EFI-pro System is a targeted further development of the successful EFI interface and enables the mobile robot to be protected in an intelligent manner. The industrial Ethernet-based EFI-pro network technology exchanges and transfer safety and non-safety data at all communication levels. The central component is the EFI-pro gateway, which ensures safe and fast networking as well as direct integration of robot controllers into the Flexi Soft safety controller via EtherNet/IPTM CIP SafetyTM. The Safe EFI-pro system therefore represents a decisive step forward for digital transformation.
Together into the future
For Martin Däumler and Meik Kettinger, Key Account Manager Electronic & Solar at SICK, the technical maturity of the solutions from SICK are a good reason for future collaboration: “Our R&D is a dynamic process. SICK is an ideal partner, especially when it comes to technical requirements, the preparation of requirements specifications, and fast response times to queries and when exchanging ideas,” describes Däumler and Kettinger adds: “We grow with our customers at each new challenge – that’s what drives us each and every day!”
The basis for a successful cooperation is in-depth knowledge and a high level of technical expertise – a certain long-standing flexibility. The partners can then jointly follow the path to success into the future. The continuous advances in mobile robotics are not limited to just the semiconductor industry but are happening in other industries too. We therefore look forward to the challenges of tomorrow and are ready to transfer our shared know-how to the pharmaceutical industry or medical technology as well.
Read more
Mobile robot revolutionizes work in supermarkets
Ultracompact mobile robots optimize the process chain
Light at the end of the tunnel - disinfection using UV light and nanoScan3
Cobots Claus and Clara: collaborative robotics with a SICK safety
Mobil robotlar:
Move into new dimensions
Robot teknolojileri yola koyuluyor – üretimde, lojistikte veya hizmet alanında fark etmeksizin. Tüm mobil robot çeşitleri için sensör çözümleri