In metalworking industries, one of the most automated equipment family are the machine tools and metal forming machineries. Machines tools fabricate parts by grinding and cutting, while metal forming machines form parts by forging, pressing, punching, bending and shearing. Many types of sensors, such as ultrasonic sensors, vibration sensors, rotary encoders, photoelectric sensors, are deployed to manage, position, and control the automated tasks. One of the most widely used are the contactless inductive proximity and the magnetic cylinder sensors, whose key roles are to check motion limits, detect positions, feedback angular movements etc.
This whitepaper discussed the possible applications of analog proximity sensors and magnetic position sensors in metalworking machineries
1.1 Analog Proximity Sensors simplifies machine control
Machine tools and metal forming machineries have rotary tasks in their automation processes. Most of the time, ro-tary encoders are used to decode information on the angular displacement. Sometime, several proximity sensors can be utilise in binary technique, e.g. 00, 01, 10, 11, to decode rotary shaft information if the application is not too concern on the precision. One other optimum way is to use an analog inductive sensors to capture higher precision angular position sensing and measurement.