Every movement in sight: The camera-monitored assembly facility at RIBE Anlagentechnik

2022-feb-09

Quality assurance through programmed imaging: The Schwabach company RIBE Anlagentechnik develops innovative assembly systems, including inspection systems, for bumpers. SICK´s machine vision helps to identify the individual components and monitor each work operation. This particular system concept could prove revolutionary for other manufacturers and suppliers as well.

Quality assurance through programmed imaging at the Schwabach company RIBE Anlagentechnik
Quality assurance through programmed imaging at the Schwabach company RIBE Anlagentechnik

The higher the level of individualization in the production areas, the more important special-purpose systems with innovative potential become. RIBE Anlagentechnik has specialized in particular in delivering added value to its end customers. The company has demonstrated its specific strengths in the technologies associated with assembly and inspection systems for the vehicle interiors/exteriors sectors and related components. Managing Director Dietmar Heckel regards the cobot and robot technologies with innovative Industry 4.0 solutions and digitalization concepts not only as a supporting pillar of RIBE Anlagentechnik but also as a cross-sectoral growth field.

Componentized construction and its modular design has become fully standardized during recent years. According to Tobias Magg, Project Manager at RIBE, it has become increasingly important to inspect individual components in assembly systems. That’s why they now offer for the vehicle and machine building industry a final assembly system for bumpers that checks, step by step, whether the correct parts for the specific bumper have been selected and mounted. The worker sees the result directly and clearly on the screen in front of him.

 

More individuality necessitates more quality control

Whether it be reversing cameras or windshield wiper systems, there are almost always multiple options available for a car model – and that means numerous bumper variants in different combinations. “The potential for error in assembly is steadily increasing as a result,” states Tobias Magg. Every post-sale correction would not only be expensive but also detrimental to the quality image of the manufacturer. In the early stages of his collaboration with RIBE, Walter Spiegel, sales engineer at SICK, called on the help of an application engineer. The aim was to literally illuminate the task. “The key issue was: We needed to bring in more light”, he said in reference to the assembly system. Many cameras that we first considered produced indistinct contrasts in this demanding and small part environment with dark parts on a black bumper background. The enormous light and therefore visual sensitivity of the Inspector P642 2D vision camera was therefore one of the decisive factors in the end for RIBE selecting that device.

Vision
Snabb och flexibel – för inspektionsuppgifter med hög hastighet
InspectorP64x
The Inspector P642 2D vision camera with enormous light and visual sensitivity
The Inspector P642 2D vision camera with enormous light and visual sensitivity

 

The large camera distance covers a wide field

The camera is located at an adequate distance of 110 cm above the bumper on the workbench and therefore outside the area where it could pose a hindrance. The worker can now install adapters, hoses, cameras and other electronics on the inside of the bumper without any risk of bumping into the camera. Using just three cameras, a very large field of view looking down on the complete bumper can be created. This is another reason why the issue of illumination was so decisive.

Tobias Magg pointed out the convenience this brings to his customers: “The standard sensor technology in the past required a large number of optic fibers or individual sensors.” Or multiple cameras with backlighting and additional illumination units. The new solution is also flexible enough to cater for the following requirements.

From the left: Tobias Magg, Project Manager Mechanical Design at RIBE Anlagentechnik GmbH; Walter Spiegel, Regional Account Manager at SICK Vertriebs-GmbH.
From the left: Tobias Magg, Project Manager Mechanical Design at RIBE Anlagentechnik GmbH; Walter Spiegel, Regional Account Manager at SICK Vertriebs-GmbH.
From the left: Tobias Magg, Project Manager Mechanical Design at RIBE Anlagentechnik GmbH; Walter Spiegel, Regional Account Manager at SICK Vertriebs-GmbH.
From the left: Tobias Magg, Project Manager Mechanical Design at RIBE Anlagentechnik GmbH; Walter Spiegel, Regional Account Manager at SICK Vertriebs-GmbH.

 

Image-guided assistance

Stefan Hochhäuser, Product Manager at SICK, was also involved in the project. “As soon as the worker moves away from the workbench to fetch the next component, he triggers an inspection of his work and thereby initiates the next work step.” The movements are detected by the small TiM100 2D LiDAR sensor which has a field of view of 200°. This compact sensor monitors the area in front of the assembly system and was a simple and cost-effective solution for RIBE, among other things because it is easy to integrate into the system and delivers stable measurements of the movements of the worker.

With the help of the triggering by the TiM100 2D LiDAR sensor and the InspectorP642, it is possible to immediately detect whether the correct part has been properly installed.
With the help of the triggering by the TiM100 2D LiDAR sensor and the InspectorP642, it is possible to immediately detect whether the correct part has been properly installed.

With the help of the triggering by the TiM100 2D LiDAR sensor and the InspectorP642, it is possible to immediately detect whether the correct part has been properly installed. In the event of an error – indicated in red on the screen – the next work step cannot be initiated. “If the inspection result is positive, the next step is displayed automatically to the worker,” says Hochhäuser. It is no coincidence, therefore, that the product was named “Inspector”.

Furthermore, each part takes about a minute to install for the worker, who wants to progress quickly and ergonomically. Thanks to the contactless job triggering, it no longer requires dozens of button presses to start and stop the camera. This saves seconds, which adds up to valuable time and cost savings over the course of a workday.

The movements are detected by the small TiM100 2D LiDAR sensor which has a field of view of 200°.
The movements are detected by the small TiM100 2D LiDAR sensor which has a field of view of 200°.

 

Quality inspection via an app in the sensor

A further prerequisite for higher productivity lies in the sensor itself, more specifically in its Quality Inspection App. It enables RIBE to configure a variety of inspection tasks in advance. For example, the sensor continuously checks whether the job was carried out correctly. This streamlines the programming in the PLC because the sensor signals the result to the controller via a TIA (“Totally Integrated Automation”) portal. This is displayed to the worker by color highlighting on the screen. In the case of a positive inspection, the task is switched or advanced. The app therefore makes it easier for customers to get started in image processing. “The parameterization in the sensor makes it simple for us to create the inspection task in the vision sensor”, says Tobias Magg. It is theoretically possible to define up to 16 jobs (inspection tasks) in a single camera.

The SICK software is equally suitable for the smaller and larger vision cameras. “If RIBE ever wants to implement the concept somewhere else, we don't have to change anything on the software side,” says Stefan Hochhäuser. “You can extract the parameters and easily transfer them to another device in the product family.” The exciting thing about this solution is its general flexibility when it comes to future developments for other components and inspection tasks. “We now have a foundation for further applications beyond assembling bumpers, says Tobias Magg.

RIBE Anlagentechnik will also have the capability in future to implement efficient manufacturing and quality inspection solutions based SICK´s machine vision, thereby providing visibility beyond the controller screen alone.

Read more

3D camera technology solves headache for packaging company

Read more

Turnkey vision solution: Looking down the barrel of a bottle

Read more

Har du frågor?

Kontakta våra experter

SICK gör vision åtkomlig
Customizable and easily configured 2D and 3D machine vision solutions – driven by SICK AppSpace
SICK gör vision åtkomlig
Customizable and easily configured 2D and 3D machine vision solutions – driven by SICK AppSpace
SICK gör vision åtkomlig

2D- och 3D-bildbearbetning konfigureras individuellt och enkelt – tack vare SICK AppSpace

Ta reda på mer