Key Takeaways
Cybersecurity has played a major role at SICK since 2018. Our holistic approach covers the entire life cycle of our products and solutions.
- Our SDL and our cybersecurity organization are certified in accordance with IEC 62443-4-1
- Our in-house testing laboratory is accredited by the German Accreditation Body (DAkkS)
- We play an active and guiding role in various cybersecurity committees
- Open-source tool QuBA libre for risk assessment in accordance with CRA
Cyber Resilience Act
Even though the Cyber Resilience Act will not be fully implemented until 2027, this does not mean that it only affects products that are developed after the effective date. The decisive factor is whether the product contains digital elements.
SICK is currently evaluating the entire affected product portfolio and implementing appropriate measures. In addition, the cybersecurity requirements for suppliers of product-related components are being redefined. We communicate product modifications resulting from these measures transparently.
As part of this review process, SICK, together with the Fraunhofer Institute for Applied and Integrated Security (AISEC), has developed the risk assessment tool “QuBA-libre”. This enables sensors, EDGE devices, and simple systems to be evaluated even during the development stage. The open-source tool provides recommendations on how to mitigate identified risks.