EN
Country: EN (Mexico)
Select country/region

Language

  • English
  • Spanish
SHDDM_01_IM0101839_1920x1080_72dpi.jpg

safeHDDM®

The innovative scanning technology

Reliable measurement accuracy of safety laser scanners thanks to safeHDDM® technology

The microScan3, nanoScan3 and outdoorScan3 safety laser scanners from SICK offer decisive advantages for plant availability and productivity thanks to the innovative safeHDDM® scanning technology. 

safeHDDM® is based on the proven HDDM (high definition distance measurement) method and is setting a new benchmark in the evaluation of optical time-of-flight measurements. This method patented by SICK filters and evaluates many individual pulses to deliver an unrivaled measurement result for a safety laser scanner.

This is how safeHDDM® ensures a very high resistance to dirt, dust, and ambient light. The most important part: safeHDDM® retains its reliability. Even an object with a reflection factor of just 1.8%, for example black suit pants, is safely recognized by the laser scanner.
And that’s not all: outdoor safeHDDM®, a further development of the scanning technology, enables the laser scanner to be used in outdoor areas. As a result, the outdoorScan3 is the first safety laser scanner to be certified for outdoor applications.

ADVANTAGES AT A GLANCE

Safe even with difficult to detect surfaces

Safe even with difficult to detect surfaces

Resistant to dirt, dust and ambient light

Resistant to dirt, dust and ambient light

Precise with 80,000 beams per minute

Precise with 80,000 beams per scan cycle

Solutions from SICK for reliable distance measurement based on the optical time-of-flight measurement principle

With optical time-of-flight measurement, the sensor emits a pulse beam that hits the target object and then is reflected back. The time that the beam takes to make this journey is evaluated and the distance to the object calculated. microScan3, nanoScan3 and outdoorScan3 typically execute a scan cycle in 40 milliseconds. Thousands of single pulses can be filtered per scan cycle. These single pulses are used by the safety laser scanners to calculate up to 2,750 reliable measured values.

SUCCESS STORIES

OUR SOLUTIONS AT A GLANCE

Let’s go: Select your product from our comprehensive portfolio

Find out more about safety laser scanners