Cruise boom continues unabated: Making cruises greener with SICK

17-07-2023

Cruises remain growth drivers and the shipbuilding industry even records two-digit growth figures in view of increased Chinese market presence. At the same time, new quality standards are quickly coming into play with regard to maritime climate protection and human and machine safety on board. SICK is supporting this wave of innovation with high-quality, technological solutions. 

 
Today part one of our three-part series on cruises with the focus on "Making cruises greener":
Passenger numbers on cruise ships are rising and maritime climate protection is becoming more important.
Passenger numbers on cruise ships are rising and maritime climate protection is becoming more important.

Vacations at sea remain attractive: Passenger numbers are increasing and new cruise ships are becoming larger and larger with capacities of up to 10,000 passengers and a crew of around 2,500. In addition, the industry strongholds in the USA and Europe will be faced with increased competition as China further drives demand for cruise ships. The main reason behind this is the “China 2025” agenda, with which China has set itself the goal of becoming the global leader in the construction and operation of cruise ships. So the “Made in China” strategy no longer just applies to building container ships – with these cruise ships for the high seas, the PRC is continuing to make gains in the most complex and technically demanding area of specialty shipbuilding. Furthermore, China’s high-income middle class is growing and more and more families are choosing to spend their vacations at sea. Destinations in Asia are also of interest to European travel providers. 

New cruise ships are being built with capacities of up to 10,000 passengers and 2,500 crew members.
New cruise ships are being built with capacities of up to 10,000 passengers and 2,500 crew members.
New cruise ships are being built with capacities of up to 10,000 passengers and 2,500 crew members.
New cruise ships are being built with capacities of up to 10,000 passengers and 2,500 crew members.

Many dreams come true on cruises. That is why cruises are one of the most attractive offers for tourists. In order for this to remain the case and so that their fleets can remain competitive, shipyards and ship owners are continuously perfecting their cruise ships and implementing new ideas. The need for action across the entire supply chain in the cruise industry is increasing dramatically. Just as comfort and entertainment options on board are on the rise, so too are the demands for increased efficiency and safety. On top of this, the logistics workload must be processed quicker and with more flexibility. Ever-more driverless vehicles are being used for this reason, such as in baggage logistics. These autonomously driving robots must be secured to avoid accidents. Monitoring the gas consumption of propulsion systems and reducing the CO2 footprint have become a natural part of climate protection 

Monitoring the gas consumption of propulsion systems and reducing the CO2 footprint have become a natural part of climate protection
Monitoring the gas consumption of propulsion systems and reducing the CO2 footprint have become a natural part of climate protection
Monitoring the gas consumption of propulsion systems and reducing the CO2 footprint have become a natural part of climate protection
Monitoring the gas consumption of propulsion systems and reducing the CO2 footprint have become a natural part of climate protection
 

Making cruises greener

Now it is not only climate activists and residents around ports who are actively reacting against ship exhaust gas emissions. Passengers also want to travel with a clear conscience on clean ships. The energy revolution has already advanced a great deal on cruise ships and ship owners often anticipate legal regulations when they introduce innovations. 

Virtually all newly built cruise ships use liquid natural gas (LNG) for propulsion, since LNG has lower emissions than marine diesel or heavy fuel oil. Moreover, the first zero-emissions ships are in the planning stages. Cleaning technology reduces the exhaust gas pollutants on older ships. SICK is renowned across the world for measuring ship emissions. Certifications from the seven largest classification organizations, which together represent more than 90% of the world’s shipping fleet, makes MARSIC from SICK the most-approved ship emissions measuring device on the market. The device measures sulfur- and carbon dioxide at scrubbers as well as nitrogen oxide before and after catalytic converters (SCR). All of this is done reliably and with very low maintenance, even during storms and high swells. The MARSIC also remains on an eco-friendly course when measuring methane if dual-fuel engines use LNG as fuel. Strict pollutant limits are also expected for soot emissions in the future. Since the corresponding technologies are already available for this, targeted solutions can already be implemented today. For example, soot particulate filters in the off-gas system demonstrably reduce the particulate mass. Even just monitoring the soot values is worthwhile for this reason, since it can be used to control motor power and save fuel. SICK has a wide range of measuring technologies that deliver reliable results, even in hot and humid exhaust gases.

 

Gasanalysatorer
Monitoring of gas as well as dust emissions on ships
Monitoring of gas and dust emissions on ships.
Monitoring of gas as well as dust emissions on ships
Monitoring of gas and dust emissions on ships.

 

Read more

MARSIC280 and Digital Services: Full steam ahead in emissions measurement technology

Read more

MARSIC emission measuring device ensures greater transparency on the world's oceans

Read more

The products
featured in this
article are now
supplied by Endress+Hauser.

Click here for the products on endress.com