149 zettabytes - or 149 billion terabytes: that's how much data was generated worldwide in 2024. According to estimates, this figure is set to rise to 527 zettabytes by 2029. But a lot of data is no guarantee of efficient processes. It can be difficult to integrate and utilize that data, especially when it comes from different sources. Digital twins are intended to remedy this situation.
Basis for interoperability
A digital twin is the data image of an asset. An asset can be many things: a product, a software program, an order and even a machine or a component such as a sensor. The asset information is semantically described and made accessible in the so-called Asset Administration Shell (AAS). As a common technical basis, it creates the prerequisites for smooth data exchange and interoperability.
The AAS was initiated by the Industrial Digital Twin Association (IDTA). This alliance, in which various industrial companies are represented, is also continuously further developing the technology. As an active member of the IDTA, SICK not only contributes its technical knowledge to the development process, but also the perspective of our customers. After all, the digital twin technology only creates real added value through specific applications.


Asset Administration Shell
An AAS consists of a series of sub-models that describe the features, characteristics, states, parameters, measured data and capabilities of an asset. Depending on the sub-models, different applications arise. SICK has already implemented various sub-models for its portfolio. SICK's digital twin infrastructure enables machine-to-machine interaction between the customer and manufacturer and follows the IDTA specifications. This makes it possible to continuously optimize customer processes and applications. And additional applications can be developed and added thanks to the modular structure of the AAS.

Product search
The search for a suitable component for a particular application can be very tedious. Technical data must first be compiled. A digital twin that is stored in a product life cycle management or engineering tool simplifies this process considerably, as the relevant data is already available in a structured form.

Master data maintenance
A precise overview of the assets used is essential for processes such as maintenance or purchasing. Maintaining such master data often involves a great deal of manual effort and is also prone to errors. Thanks to the standardized form of the AAS, the data can be entered digitally into a variety of systems.

Product Change Notification
Due to the increasing networking and digitalization of many processes, the speed at which updates and patches are released has increased. Especially when it comes to critical, safety-relevant updates, action must be taken quickly. With AAS, such changes can be communicated manufacturer-independently and interoperably from component manufacturers to machine builders and end customers.

Further sub-models such as simulation under development
We are also constantly evaluating and developing further sub-models for additional applications. This includes, for example, a model for the simulation of a sensor. This allows a component to be tested and the configuration optimized as early as the design phase. This then speeds up the actual commissioning. We have developed such a model, for example, for our W12 series of photoelectric sensors, and more are in the works.

Virtual sensor solutions for NVIDIA Isaac SIM
The simulation models from SICK are also available for NVIDIA Isaac Sim. We rely on OpenUSD as an open standard for the exchange of 3D models and as the basis for realistic sensor simulation. The SICK products are publicly available for Isaac Sim users. The virtual portfolio includes LiDAR sensors and 3D and 2D camera models for safety and non-safety applications. The portfolio is being continuously expanded to provide users with a growing range of solutions for simulation, validation and AI training.