Privacy policy for the development of a camera system for detection of persons

SICK 欢迎您访问我们的网站,感谢您对我们企业、产品和服务的关注。保护您的隐私是我们的重要责任,我们希望您安心访问我们的网页。为此,我们将在下方说明访问我们网页期间将处理哪些信息。

Responsible SICK AG, Erwin-Sick-Straße 1, 79183 Waldkirch, Germany
Purpose of processing Development and validation of a system for safeguarding hazardous areas
Categories of data
  • Image data
  • Video data
  • 3D information
  • Time of recording
  • Identification of the recording unit
  • Camera settings
  • Diagnostic information
The quality of the video material allows people to be identified in particular, but not exclusively, when the person's gaze is directed towards the camera system.
Legal basis GDPR Art. 6 (1) f) - legitimate interests
Legitimate interest SICK processes image, video and 3D data in combination with the above-mentioned additional information for the training and validation of AI systems and for the validation of deterministic algorithms. Most of the data is processed automatically. This processing is done to protect people in the vicinity of machines and to prevent accidents involving them. By developing such a system for the protection of persons, there is a justified corporate interest in the general welfare of all persons. The purpose of the system's accident prevention therefore means that future protection in the interests of all people outweighs the right to the image recordings of the individual, which is worthy of protection.
Consequences of failure to provide the data None.
Storage duration The data will initially only be stored until the end of the first test phase (April 30, 2025). Storage of the data beyond this date is only possible in consultation with the works council and prior notification of the persons concerned.
Data source Direct collection of data through image / video recording.
Recipients of the data Certifying bodies
Transmission in third countries We do not transfer any personal data to third countries.
Logic of the automated decision We do not make automated decisions that may have consequences for data subjects.

 

您的权利

您有权

  • 了解相应的个人相关数据;
  • 修改相应的个人相关数据;
  • 删除锁定相应的个人相关数据;
  • 反对处理相应的个人相关数据;
  • 传输相应的个人相关数据;
  • 如果处理相应的个人相关数据是基于您的同意,则日后可撤回同意;以及
  • 只要您认为相应的个人相关数据处理违反数据保护法,可向数据保护监督机构投诉

对此请联系数据保护专员。我们将妥善答复所有请求。

隐私条款修改

我们保留随时根据适用要求调整隐私条款的权利。可在我们的网页中随时调阅当前的隐私条款。