Detecting road damage using LiDAR sensors

30 oct 2023

There are about 51,500 kilometers of asphalted roads in Finland. Around 8,000 kilometers of the roads were in poor condition at the end of 2022. The underlying causes of the damage can be determined with the help of the measurement and analysis technology for roads and paths developed by Roadscanners. This enables preventive measures to be initiated to reduce the costs in the life cycle of a road.

Car standing on the road
Car standing on the road

Advice, software and devices from Roadscanners

Roadscanners is a global company for advice, software and the sale of research and measurement equipment for managing and maintaining traffic infrastructure. It focuses on the monitoring and analysis of the condition of roads, paths, bridges and airports. The method employed by Roadscanners has proven efficient both in the inspection of road networks in small municipalities as well as in larger road networks covering thousands of kilometers. The bigger the road network, the greater the potential savings.

The RDLS Grid technology used is also employed for laser scanning of power lines from helicopters to avoid storm damage. It enables areas to be identified where trees or vegetation need to removed to avoid storm damage from falling trees.

Digitizer stands in front of a plane
The detecting device "Digitizer" in action.
Digitizer stands in front of a plane
The detecting device "Digitizer" in action.

Analysis by video, ground radar, laser scanner or thermal imaging camera

The research and analysis technologies used by Roadscanners include video, ground radars, laser scanners, thermal imaging cameras and accelerometers. The ground radar can penetrate up to three meters under the road surface. The road surface above the ground, including the embankment, is analyzed using a laser scanner. The laser scanner used by Roadscanners is a LMS5xx 2D LiDAR sensor from SICK. Currently, either one or two simultaneously operating laser scanners are used in the vehicles depending on the measurement requirements. The speed of the measurement vehicle is about 30–80 km/h.

The rugged 2D LiDAR sensors are ideally suited for this application because it is very easy to integrate the software into the device. Jani Irvankoski from Roadscanners remembers that his first coding task 13 years ago was to integrate a laser scanner from SICK – to this day he cannot recall any device failures occurring. The collaboration with SICK has proven very successful, and the responsible sales manager Villa Sarviaho is on site to present the trends and new product developments.

Visualization of the data generated by a LiDAR.
Visualization of the data generated by a LiDAR.
Visualization of the data generated by a LiDAR.
Visualization of the data generated by a LiDAR.

Responding before the damage is even visible

The most common and greatest risk factor for damage to the road surface is water. When the subgrade is wet, the load bearing capacity of the road is reduced and it is more susceptible to damage. The snow walls on the side of the road in winter, for example, should be cleared in a timely manner to ensure water does not penetrate into the road subsurface when it melts.

60–80% of road damage occurs in the spring when the road is most susceptible.
Typical structural problems are caused by heavy traffic on road sections with a thin pavement and poor subgrade.
60–80% of road damage occurs in the spring when the road is most susceptible.
Typical structural problems are caused by heavy traffic on road sections with a thin pavement and poor subgrade.

The measurements of the roads and road surroundings using 2D LiDAR sensors were carried out in spring before the roadside ditches are covered in vegetation, which would make it more difficult to take precise measurements of the depth of the ditches.

A further advantage of precision laser scanning is its repeatability, which makes it possible to monitor groove formation and the condition of the ditch bottom through repeated measurements, for example from year to year. Changes can then be responded to in a timely manner before serious damage to the road occurs. The repairs are then also less costly as a rule.

 

An eye on the changing seasons

The change of seasons and the freeze-thaw cycles are some of the most important factors that affect the condition of the roads in cold regions. 60–80% of road damage occurs in the spring when the road is most susceptible. Typical structural problems are caused by heavy traffic on road sections with a thin pavement and poor subgrade. Maintenance defects can generally be attributed to defective draining and inadequate winter road clearance.

 

Read more

Safety expertise for implementing innovative Smart City projects

Read more

Artificial intelligence ensures traffic safety in the San Bernardino road tunnel

Read more