Presse Salons: ACHEMA 2015

More than 166,000 trade show visitors learned about new technologies at the ACHEMA. As one of the 3,813 exhibitors at the event, SICK showcased its solutions for process technology with its slogan ... Lire la suite
With the MCS300P, SICK has produced a compact device with proven measurement technology specifically for process gases. The multi-component analyzer system for high-quality products provides ... Lire la suite
With its LFP Cubic and LFP Inox level sensors, SICK is offering solutions that are suitable for any application, in any setting – whether it involves continuous level measurement, point level ... Lire la suite
The SICK flame ionization detector represents both a compact analyzer and a professional device for continuous hydrocarbon measurement. The GMS800 FIDOR combines rugged design, simple operation, ... Lire la suite
The FWE200DH represents SICK's next stage in the development of a dust measuring device for measuring dust concentration in wet gases. The gas is extracted via a sampling probe and heated above dew ... Lire la suite
The FLOWSIC500 ultrasonic compact gas flow meter from SICK is specifically designed for natural gas distribution applications requiring verified calibration. It ensures precision charging, making ... Lire la suite
The EuroFID3010 total hydrocarbon analyzer from SICK is a heated flame ionization detector for determining the volatile organic compounds (VOC) in exhaust air and exhaust gas. It is currently the ... Lire la suite
With the deTec4 Core Ex, SICK is setting a new standard for safety light curtains in explosive environments. Combined with the explosion-protected enclosure, it can be used in industrial sectors ... Lire la suite