The data is there. Sentio lets you recover the treasure.
Accueil Annual Report 2025 Sentio
Data is the raw material of Industry 4.0. But many companies still aren’t putting it to use. The individual systems are too different, integration often too complex. With Sentio, SICK intends to change all that. In the future, the platform will integrate sensors, machinery, and IT to create an easy-to-use system that makes all data leverageable at a glance. The resulting increase in performance through Sentio will be immense.
“We want to make it as easy as possible for customers, with as few gaps as possible,” says Jan Glaeser. The Senior Manager Marketing – Integration Automation often explains how Sentio works by way of a comparison. Think of the industrial Internet-of-things platform like the control hub for a smart home, Glaeser suggests. A control hub collects all the data from a networked house. Sensors measure how much electricity the fridge and heat pump are using, they know the temperature inside the house and the output of the solar panels. This data is used to control the technology as efficiently as possible with the help of AI.
Like a smart home, Sentio collects data from industrial facilities: running times, RPMs, quantities, energy use, and operating states. On top of that is data collected by the sensors: temperature, pressure, position, vibration, fill level, and object detection. Positioning data and process data complete the picture. This data can be integrated into IT systems, preferably via open protocols or easily with SICK ConnectX. Open standards are used wherever possible, such as IO-Link for sensor data or omlox for localization and position data. This establishes a foundation for interoperable use on the customer’s premises. Sentio visualizes and analyzes this trove of data and provides specific recommendations for action.
For example, the solution enables you to trace a component throughout the production process in real time. It also detects early signs of equipment wear and tear and provides recommendations for proactive maintenance. Faster and more exact process optimization improves performance, improvements that can also be achieved by using a digital twin.
“Sentio allows us to combine an extremely heterogeneous world of sensors, systems, and data to a comprehensive solution,” says Glaeser. This makes data accessible and usable all at once, data that used to be very difficult to leverage. Think of it like a huge treasure trove that sank at sea. Sentio is like a submarine, crane, and digital control hub all at once – a system that can recover treasure in a few simple steps. After all, data is a treasure trove. “We make this treasure accessible in the first place – and then usable,” says Glaeser.
Sentio’s intuitive IIoT platform combines engineering, integration and insights, turning complexity into clarity. This offers industrial companies a one-of-a-kind opportunity. Unlike the consumer sector, where there are many common standards (USB, WLAN, etc.), the industrial sector remains prone to proprietary solutions from individual companies. With Sentio, SICK is jailbreaking these proprietary systems, at least to a degree. The treasure trove of sensor data now available gives rise to countless opportunities to improve performance.At the same time, Industrial Internet of Things (IIoT) platforms like Sentio are subject to higher requirements for robustness, service, security, and connectivity than those in the consumer sector. SICK meets these requirements with its new platform. Security updates are quick and easy to perform. This is an important promise from SICK: Customers will receive support for the entire lifecycle of their sensors and machines. This significantly contributes to investment security.
Sentio also makes it easier to operate and handle engineering tools. SICK is successively bundling the multiple engineering tools it used to offer for different applications into one single platform, Sentio, for all applications. “We used to have many individual tools; now we’re turning to a central, expandable system,” says Glaeser.
But in order to still respond to each individual customer need, SICK offers different expansions for Sentio. Customers who want to efficiently commission mobile robots in their factory can add the “Mobile Robot Manager”. This modular expansion results in direct increases in performance for customers. “Performance improves because customers get results faster,” says Jan Glaeser. Sentio supports customers in all areas of factory digitalization, from engineering and integration to data-based insights. The spectrum ranges from the efficient planning and implementation of sensor solutions to the integration of operating technology into IT environments, as well as the use of sensor data for predictive maintenance, process optimization, and informed decision-making. Sentio offers everything from a single source, with as few gaps as possible.