Indoor positioning of important assets using ultra-wide-band
Accueil Annual Report 2025 Intralogistics
There is one question that dominates Paul Balzer’s professional life: “Where are important things located?” As an engineer and product manager at SICK, Paul Balzer is responsible for the real-time location system (RTLS).
The system enables companies with complex production processes to take indoor localization to a new level. Each asset (such as tools or assemblies) fitted with a CorivaTag can be positioned to the inch in interior spaces. In this way, SICK makes possible the smart digitalization of the materials flow in addition to significant improvements in performance.
Think of the Coriva System like GPS for interior spaces. Like the Global Positioning System, there are satellites (CorivaSats) and mobile devices (CorivaTags). Objects fitted with a CorivaTag are positioned inside buildings using the wireless technology known as ultra-wide-band (UWB). A software program (CorivaEngine) calculates the positions of the mobile devices. The system works in seconds and is precise, robust, and scalable. “Coriva gives you a real-time overview of your flow of goods,” explains Paul Balzer.
Paul Balzer completed his training as a surveying technician. He then studied automotive engineering, completed a postgraduate course in digital signal processing, and completed a certification course titled “How to Program a Self-Driving Car”. During the course, he discovered that positioning would be a crucial aspect of future automotive applications.
But besides automotive applications and autonomous driving, positioning is also crucial in other areas as well. From autonomous vehicles in industrial environments to AI-controlled humanoid robots in production and logistics, they all need to be localizable as well as have the ability to localize one another.
Many companies today already use SICK’s indoor positioning solution to know the location of important assets at all times. One example from the field of chip manufacturing: Wafer boxes, which contain multiple extremely thin layers of semiconductor material that are often worth several million euros, are positioned with UWB technology. Another example is vehicle manufacturers, who have to prove that their vehicles have undergone bench testing. Positioning data enables this process to be logged automatically.
But it is companies with complex production processes, such as those in the automotive, machine engineering and electrical industries, that benefit most from real-time localization. This is because they are able to trace and control their tools, assemblies, products, and means of transport in real time.
“The major advantage our system offers is significantly reducing the time spent on searches and preventing mix-ups,” states Paul Balzer. Whenever a person has to manually scan an asset to record its location, mistakes can creep in. Balzer gives an example: “Imagine someone sets down a pallet in the hall. But the pallet is in the way, so another associate moves the pallet before returning to other work – next thing you know, it’s a wild goose chase.” And when the material on the pallet is urgently needed, it is impossible to overstate the advantage of real-time localization. Not to mention the efforts one saves by not having to manually scan assets.
Companies that want to make their warehouse processes, transport routes, and transport drives more efficient can also benefit from the data the Coriva System collects. The Location Management insight tool visualizes and analyzes the data, reducing empty runs and delays. Balzer gives another example: “A great number of forklifts are used in intralogistics, so transit times are high. The Coriva System and CorivaHub allow you to trace and analyze all of your vehicles, helping you find the shortest and most efficient routes between your logistics points.” By ensuring transparency, this is a boon for companies undergoing audits and inspections.
Customers also benefit from the great flexibility and compatibility of the Coriva System, which is certified according to the omlox standard. As the world’s first open locating standard for industrial localization systems, omlox also allows for the use of technologies from other providers. For more, see next page. But not every asset that you want to trace requires a CorivaTag. “The showcase skill is the ability to combine the different technologies,” says Paul Balzer. RFID gate detection, GPS-based outdoor localization, LiDAR (light detecting and ranging) positioning, and video-based positions can all be connected to the omlox hub using ultra-wide-band technology (Coriva System).
The upshot is that for companies seeking to optimize the performance of their internal materials flow, all the bases are covered.