If you order a tequila sunrise on the rooftop terrace in the TownHouse Duomo hotel in Milan, you will not get your drink served by a barkeeper made of flesh and blood, but rather from “Toni”, the cocktail robot. In a futuristic bar with more than 150 kinds of spirits which hang upside down from the ceiling, the robots expertly mixes first-class cocktails. The stainless steel barkeeper was developed by Italian robot maker company MAKR SHAKR. The robot gripper arms are from KUKA, the intelligent safety concept for direct human-machine collaboration from SICK.
Shaken, not stirred: Makr Shakr, KUKA and SICK are mixing cocktails
The robotic barkeeper – which goes by the name of Toni – is fully-automatic and, using his robot gripper arms. He pours tequila, lemon and orange juice, fills the cocktail shaker with ice cubes, shakes it powerfully, carefully adds grenadine, decorates the tequila sunrise with a slice of lemon and serves it to the guest. The cocktail robot can mix anything, from classic gin tonics to special creations. However, he needs precise instructions and the order must be made by clicking in a tablet app. He then gets started and servers freshly-prepared cocktails at a consistent level of quality completely on his own.
The openly-accessible working range is protected by four safety laser scanners from SICK during the entire mixing process. There are two S300 on the front side and one safety laser scanner on each the left and right side.
Read more:
The new mobility: How sensors control the cobots of the future
Robot Operating System (ROS) with SICK and KEBA: Diversity and simplification
3D localization with the Belt Pick SensorApp for pick-and-place tasks
Part localizer from SICK brings order to the chaos of mixed-up parts
Making hard things easy – a safety solution for a mobile heavy-load robot
colaboração em nível igual
Quer se trate de Robot Vision, Safe Robotics, End of Arm Tooling ou Position Feedback – os sensores da SICK capacitam o robô para uma percepção mais precisa.
Descubra mais