User-friendly configuration of EtherNet/IP encoders

21/jun/2013

Using the function blocks specifically developed for integration of the AFS60 and AFM60 EtherNet/IP encoders into Rockwell controllers allows retrieving, reading, and partly writing (set and get) pre-installed parameters such as resolution, counting direction, or velocity format directly from the controller. Moreover, one can configure numerous additional functions, e.g., temperature monitoring, threshold values, or the operating hours counter with a few clicks. This provides the user with maximum convenience when installing the EtherNet/IP encoders.

 

WebServer and FTP update extensions for even more user-friendliness

AFx-Ethernet / IP Encoder

AFx60 Ethernet/IP Encoder

The function blocks for integration of the EtherNet/IP encoders, supplied by SICK as the only producer so far, will in the future benefit from two interesting extensions of the AFS60 EtherNet/IP and AFM60 EtherNet/IP encoders, respectively. In case of format adjustments or batch changes, for example, the WebServer functionality enables the user to modify encoder parameters directly via the operator interface of the machine - without any intervention in the often complex program structure of a control unit. Extension of the EtherNet/IP encoders from SICK by an integrated FTP bootloader makes it possible to update the encoders at any time with the latest firmware right in the plant, without having to replace the sensor for this purpose.