EN
Country: EN (Belgium)
Select country/region

Language

  • French
  • Dutch
  • German
  • English
separation-distance-stage-teaser-image-webx

What‘s new with ISO 13855:2024?

All you need to know!

Keeping up with the latest developments regarding Separation Distance

With the release of the updated ISO 13855:2024 standard on November 21, 2024, the topic of separation distance has undergone substantial improvements. These modifications affect anyone who designs, validates or inspects safety solutions, striving to create a safe work environment for existing machinery that may be used by workers without impairment to their safety or health.

What are the most relevant alterations? And what do you need to consider to comply with the requirements? Safety experts from SICK provide support in finding answers to all these questions.

What's new with ISO 13855:2024?

The new ISO 13855:2024 standard includes some significant amendments. Terminology and variables have been updated to represent concepts more clearly, terms have been made more precise, and new content – such as additional protective devices and additional distances due to tolerances relating to the measurement principle – has been added. These revisions require adjustments in the market and by designers of new equipment.

A woman points to the word "standards", which is depicted with many other holograms.

How you can benefit from the new regulations

The market benefits from a more comprehensive design through the integration of protective devices not previously addressed and the consideration of additional distance factors that enable safety concepts to be further optimized. The standard provides valuable benefits through improved specifications and more precise requirements for the selection, configuration and placement of protective devices. These enhancements will contribute to better safety solutions that enhance safe productivity and lower the total cost of ownership.

A safety expert checks the functionality of a safety device

SICK supports you in the implementation of the new standard

SICK safety experts have prepared a comprehensive poster that shows at a glance the requirements for sensitive protective equipment (SPE) in the new ISO 13855:2024. This comprehensive overview also addresses equivalent presence-sensing device requirements which have been updated in North American standards, namely ANSI B11.19-2019 (which was recently reaffirmed in December 2024). The aim is to give designers clear and concise information so they can quickly and efficiently adapt to the new standards. Furthermore, SICK provides specific training, technical support, and tailored solutions that make it easier to implement the specifications and optimize the safety of machinery.

One safety expert takes measurements on a machine, a second one takes notes

CONTACT US!

Do you have questions about separation distance?  Our experts will be happy to help you and find the right solution for you.

Contact form with envelope symbol

Contact

Guide: Enhancing Separation Distance Competence

The Global Separation Distance Guide compiled by SICK Safety experts provides background and guidance on dimensioning and positioning safeguards in line with the newly revised safety standards [ISO 13855:2024, ANSI B11.19-2019 (R2024) and CSA Z432:23]. It provides detailed information for determining separation distance, highlights key regional differences and supplements the step-by-step poster with further explanations.

By providing detailed guidance for designing, implementing and verifying safeguards fulfill distance requirements, this guide helps to effectively reduce risks in line with the latest findings on the factors to be considered, thereby improving safety and health in the workplace.

Download now
The poster is displayed as a preview on a tablet and laptop monitor

Poster: Separation Distance step-by-step

Safety experts from SICK have compiled the requirements of Separation Distance in a step-by-step overview poster. Instructions from both ISO 13855:2024 and ANSI B11.19-2019 are provided. The poster summarizes the key aspects and, based on the approach direction to the detection zone and the particular reference plane, guides the user through the process of appropriately selecting the respective criteria that need to be considered with respect to dimensioning and positioning.

Download now
The poster is displayed as a preview on a tablet and laptop monitor

Webinar: Watch recording now

What are the key changes regarding separation distance requirements?

Learn from our safety expert what you need to consider to meet the requirements.

Watch webinar recording here