SICK Austria awarded with ALC (Austrian Leading Companies)

Since 1997, SICK Austria is located in Wiener Neudorf and successfully contributes to the regional business. Due to the financial success, the company received position 3 in the category international companies at the ALC (Austrian Leading Companies) contest. With this placement, SICK Austria counts as one of the most successful companies in Lower Austria.

The award concentrates on the corporate success. It shows the innovative power of SICK Austria. The employees are an important part of the success and help to let the company continually grow. For over 20 years, “Die Presse” awards the ALC prize. In two categories, the companies are being rated. For the award, only pure numbers and facts of a company are asset by a jury.

The two categories divide into location and focus of operations. One category includes companies with a location and focus in Austria. The second category includes companies, which are located in Austria with international focus of operations. Furthermore, the two categories subdivide in companies with a sales amount of 10 Mio. Euro max and companies with an amount of more than 10 Mio Euros.