Contact
Feedback

Detection reliability using innovative technologies

High-performance technology is the norm for the photoelectric sensors in product families W16 and W26. A wide range of innovative functions enables reliable detection of reflective, uneven, perforated, transparent and depolarizing objects:

 

 

TwinEye technology

TwinEye technology offers maximum operational safety for shiny, reflective and even jet black objects. Two receivers in one sensor provide much higher levels of detection reliability. The sensor only changes its output state if both receivers measure the same detection result. In this manner, the W16 and W26 not only reliably detect very shiny and high-contrast objects, but also uneven surfaces.

 

LineSpot technology

LineSpot technology ensures that perforated, textured, and uneven objects can be reliably detected. The light spot, which has been extended to form a line, allows optical information to be provided about irregularities, such as gaps or rough surfaces.

 

 

ClearSens technology

In the case of transparent objects, such as glass bottles or cling film, ClearSens technology guarantees the best perspective. The right detection mode can be set directly on the device according to the object characteristics and attenuation. If the reflector or the front screen of the sensor is contaminated, the photoelectric sensor automatically repositions its switching thresholds thanks to AutoAdapt, thus always providing the highest levels of detection reliability.

More sensors with ClearSens

 

 

Optical filter

The new photoelectric sensors have a high ambient light immunity which makes them immune to LEDs or reflections from high-visibility vests. They are also suitable for reliable detection of depolarizing objects such as film-covered containers or parcel tape. The signals received are similar to those from the reflector which explains why switching errors used to occur in common technological designs.

Any questions?

Ask our experts

TOP