Registration
Click here to register for Automatic Identification Systems Training. Descriptions of the avalable training sessions can be found below.
Airline Luggage Identification System (ALIS) with Remote Diagnostic Tool (RDT)
This course is designed for technicians and maintenance personnel responsible for monitoring performance and maintenance of the ALIS system.
This 8-hour course starts with basic scanner operations, specific to airline baggage systems, then covers the integration of the scanners into a system describing hardware components, cabling and component connections. Using RDT 400 on the installed system, selected displays are used to monitor run time operations and detect abnormal or suspect performance characteristics. Advanced OTC and scanner diagnostics are performed on the system along with scanner and OTC file maintenance procedures. System availability for training may impact the overall length of the course.
Technology of Reading Bar Codes
OPS Concepts and Operation
Introduction to CLV Setup
OTS Diagnostics using the Terminal Emulator
Working with Project and Scanner Files
Maintenance Practices
RDT Displays
RDT Display Configuration
Omni Portal System (OPS) with Remote Diagnostic Tool (RDT)
This course is designed for technicians and maintenance personnel responsible for monitoring performance and maintenance of the OPS system.
This 8-hour course starts with basic scanner operations, specific to your system application, then covers the integration of the scanners into a system describing hardware components, cabling and component connections. Using RDT 400 on the installed system, selected displays are used to monitor run time operations and detect abnormal or suspect performance characteristics. Advanced OTC and scanner diagnostics are performed on the system along with scanner and OTC file maintenance procedures. Component replacement procedures are covered at the installed system. . System availability for training may impact the overall length of the course.
Technology of Reading Bar Codes
OPS Concepts and Operation
Introduction to CLV Setup
OTS Diagnostics using the Terminal Emulator
Working with Project and Scanner Files
Maintenance Practices
RDT Displays
RDT Display Configuration
Baggage Dimensioning System (BDS)
This course is designed for technicians and maintenance personnel responsible for monitoring performance and maintenance of the dimensioning system.
This 6-hour course starts with an introduction to system operation and components, cabling and component connections. Using the local or remote display on the installed system, display features to monitor run time performance are covered. Advanced MHI and scanner diagnostics are performed on the system along with MHI file maintenance procedures. Component replacement procedures are covered at the installed system. System availability for training may impact the overall length of the course.
Systems Overview
Operator Interface
Description of Components
Preventive Maintenance & Fault Detection
MHI Serial Communications Setup
MHI Diagnostics and Replacement
LMS 200 Diagnostics and Replacement
Tachometer Diagnostics and Replacement
Calibration Procedures
Web Pages
MHI File Management
Remote Access Functions
Volumetric Measuring System (VMS)
Volumetric Measuring System (VMS)
This course is designed for technicians and maintenance personnel responsible for monitoring performance and maintenance of the dimensioning system.
This 6-hour course starts with an introduction to system operation and components, cabling and component connections. Using the local or remote display on the installed system, display features to monitor run time performance are covered. Advanced MHI and scanner diagnostics are performed on the system along with MHI file maintenance procedures. Component replacement procedures are covered at the installed system. . System availability for training may impact the overall length of the course.
Systems Overview
Operator Interface
Description of Components
Preventive Maintenance & Fault Detection
MHI Serial Communications Setup
MHI Diagnostics and Replacement
LMS 200 Diagnostics and Replacement
Tachometer Diagnostics and Replacement
Calibration Procedures
Web Pages
MHI File Management
Remote Access Functions
Volumetric Measuring System (VMS)
Camera System Operations
This course is designed for technicians and maintenance personnel responsible for monitoring operation and performance of the system. This is also a prerequisite for Camera System Diagnostics and Maintenance.
This 3 hour course starts with an introduction to system operation, components and communications. Using the local or remote display for the installed system, display features to monitor run time performance are covered. Special attention to abnormal display indications are covered along with basic fault diagnostics.
System Overview
Camera Tunnel System Components
Introduction the Tunnel Monitor
Viewing Operations using the Tunnel Monitor
Preventive Maintenance and Fault Detection
Using the Image Viewer
Tunnel and Archive Files
Camera System Diagnostics and Maintenance
This course is designed for technicians and maintenance personnel responsible for monitoring performance and performing system maintenance. Camera Systems Operations is a prerequisite for this course.
This 5-hour session consists of two major maintenance tasks: using fault indicators to locate the source of the fault and performing component replacement. When a suspect component is found, additional diagnostics can be performed to verify the fault. Students will use the manual’s detailed diagnostic procedures to verify component operation. The uncomplicated design of component mounting along with the manual’s replacement procedures simplifies component replacement. System availability for training may impact the overall length of the course.
Tunnel System Troubleshooting
Understanding Camera Log Files
Using CiMenu
Serial & Telnet Communications Setup to the MHI
MHI Diagnostics
MHI Replacement
MHI File Management
LMS200 Diagnostics & Replacement
LMS Calibration Procedures
Tachometer Diagnostics & Maintenance
Camera/Light Assembly Replacement
Camera Calibration
Modular Light Grid