Skip Navigation Linkssickusa.com > EN > Home > Public Relations > Press Releases
Print

SICK Introduces SLG Family of Light Grids 

 
Click to show / hide content block    Page Header
Show Page Header 
Show Date 
Hide Subtitle 
Show Leadtext 

2010-02-17 

Minneapolis, Minn. - February 22, 2010   
The SLG is the slimmest and sleekest light grid in its class                                                                                                                                                                                                                        
Click to show / hide content block    Content Block 01
Show Content Element 
No Links 
Hide Title 
Hide Subtitle 
Hide Image 
 

 

 

 
 

SICK (www.sickusa.com), one of the world’s leading manufacturers of sensors, safety systems, machine vision, and automatic identification products for factory and logistics automation, today announced the launch of its new SLG family of non-safety, through-beam light grids. The SLG is the slimmest light grid on the market. Using only 8 mm of space for the optics, the SLG can be hidden inside machines, frames, doors, and other places where space and aesthetics are desired. In addition to its small size and simple configuration interface, the SLG is also the lowest-cost solution for detecting an object as it moves through an area.  

The SLG family is organized into three groups:

        SGS - for large areas, such as doors and gates

        SAS - for smaller area coverage on machines and with more advanced configurations

        SPL - for pick-to-light applications with automatic teach-in and job LEDs

Additional features and benefits include one touch setup – configure and adjust sensor without a PC. Customers can also detect small objects when the cross beam function is enabled to increase resolution to 25 mm. Advanced options work to keep the sensors reliable and available. Their sleek and slender design not only saves space, it creates more work area. In addition, out-of-the way installation can prevent intentional and accidental damages. They are designed with cost-savings in mind, offering simple “break-a-beam, get-an-output” functionality. Typical applications are pallet jut-out or overhang detection on conveyer belts, opening doors for door and gate access control in factories and distribution centers, part ejection detection in wood and metal fabrication, and door control on mass transit, such as subways, busses and trains. 

Click to show / hide content block    Web Part Container
Click to show / hide content block  Content Block 02
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
Tracie Manor
6900 W 110th St
Minneapolis, MN
55438 USA
Button to start the search