Skip Navigation Linkssickusa.com > EN > Home > Public Relations > Press Releases
Print

SICK Launches OLM High-speed, Long-range Fine Positioning Sensor 

 
Click to show / hide content block    Page Header
Show Page Header 
Show Date 
Hide Subtitle 
Show Leadtext 

2010-02-17 

Minneapolis, Minn. - February 17, 2010   
Increase speed and positioning accuracy - reach positions faster with millimeter precision                                                                                                                                                                                                            
Click to show / hide content block    Content Block 01
Show Content Element 
No Links 
Hide Title 
Hide Subtitle 
Hide Image 
 

 

 

 
 
SICK (www.sickusa.com), one of the world’s leading manufacturers of sensors, safety systems, machine vision, and automatic identification products for factory and logistics automation, today announced the launch of its new OLM Distance Measurement Positioning Sensor. The OLM is used for high-speed, high-precision positioning of overhead cranes, rail and transfer cars, monorails, shuttles, elevators and other vehicles. The vehicle can be positioned around curves and inclines where traditional laser measurement systems cannot be used.

SICK has the largest and most complete offering of distance measurement and positioning sensors, offering optical laser, ultrasonic, magnetic sensors as well as and rotary wire draw and magnetic linear encoders. The OLM adds one more method of long-range fine positioning by using a linear bar code tape for positioning.  With the OLM, users can position vehicles with 0.1 mm resolution at distance up to 10 km, providing more than 6 miles of unique positions at increased speed and positioning accuracy. In addition, this non-contact solution helps ensure longer use and reliable measurement, offering the longest runtime of any positioning sensor. Its four LEDs and CMOS camera last twice as long as lasers and rotating mirror technology used in competitive sensors and positioning methods.

The OLM improves overhead crane and monorail positioning with exact absolute position information and eliminates overshooting targets, creeping into position, and re-zeroing that is standard for typical systems using rotary encoders and mechanical switches for positioning. In addition, it offers easy installation due to its integrated skew and tilt angle, ensuring fast installation, commissioning, and reduced start up time.

Click to show / hide content block    Web Part Container
Click to show / hide content block  Content Block 02
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
Tracie Manor
6900 W 110th St
Minneapolis, MN
55438 USA
Button to start the search