Skip Navigation Linkssickusa.com > EN > Home > Public Relations > Press Releases
Print

SICK Launches Inspector Viewer  

 
Click to show / hide content block    Page Header
Show Page Header 
Show Date 
Show Subtitle 
Show Leadtext 

2010-11-11 

Minneapolis, MN - November 11, 2010   
  Compact, real-time, touch-screen monitor provides advanced monitoring and trending
Click to show / hide content block    Content Block 01
Show Content Element 
No Links 
Hide Title 
Hide Subtitle 
Hide Image 
 

 

 

 
 
SICK (www.sickusa.com), one of the world’s leading manufacturers of sensors, safety systems, machine vision, and automatic identification products for factory and logistics automation, today announced it has launched the Inspector Viewer. The Viewer is a compact, real-time, touch-screen monitor that provides advanced monitoring and trending capabilities for Inspector Vision Sensors - right next to the production line.

Users will instantly get information about multiple inspections in order to improve quality and throughput. It is ideal for the packaging and food and beverage markets - monitor label inspection and logo verification via live or logged images, for example.

Features and benefits include:

 Perform trending and analysis
--The results of each of the detailed inspection tools can be monitored for immediate and visual feedback to line operators.

 View live or logged images and statistics from the Inspectors
--User can now see live image in real-time without having to connect a PC

 Viewer also allows user to view and store logged images based on the user’s criteria

 Easily re-teach the reference image to handle batch switching
--Image re-teach allows users to quickly adapt to small variations in production

 Save and export configurations from and to Inspectors
--This allows users to have a virtually infinite number of preset inspections, which increases the functionality of all Inspectors to handle large product ranges

 Continuously store images from the Inspector on the Viewer
--Save images to on-board compact flash drive with room to store up to 23,000 images

• Monitor all Inspectors on the network from a single device and location

Click to show / hide content block    Web Part Container
Click to show / hide content block  Content Block 02
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
Tracie Manor
6900 W 110th St
Minneapolis, MN
55438 USA
Button to start the search