SICK (www.sickusa.com), one of the world’s leading manufacturers of sensors, safety systems, machine vision, and automatic identification products for factory and logistics automation, today announced the launch of its DDS36 and DDS50 incremental encoders. They are low-cost, light duty optical incremental encoders that offer an exceptional price/performance ratio. The DDS36 encoders have a 36 mm housing and the DDS50s have a 50 mm housing, making them ideal for applications where space is a premium. The DDS series of encoders can be used in light duty applications that require reliable speed feedback with pulses per revolution between 100 and 2,500. With an IP 65 enclosure rating, these encoders are ideal for outdoor use, and can be used for positioning of overhead cranes, rail/transfer cars, in robotic applications, and rack and pinion arrangement material, and speed detection during critical manufacturing processes.
Key features: