Skip Navigation Linkssickusa.com > EN > Home > Public Relations > Press Releases
Print

IME Inductive Sensors Offer Exceptional Accuracy and Repeatability 

 
Click to show / hide content block    Page Header
Show Page Header 
Show Date 
Hide Subtitle 
Show Leadtext 

2009-09-15 

Minneapolis, Minn. - September 15, 2009   
  New Enhancements Provide Increased Switching Frequency and Temperature Range
Click to show / hide content block    Content Block 01
Show Content Element 
No Links 
Hide Title 
Hide Subtitle 
Hide Image 
 

 

 

 
 
 

SICK (www.sickusa.com), one of the world’s leading manufacturers of sensors, safety systems, machine vision, and automatic identification products for factory and logistics automation, today announced new enhancements to its line of IME Inductive Sensors. These enhancements include an increased switching frequency and a wider temperature rating for demanding applications in packaging, assembly, metal forming and automotive industries.

IME sensors are ideal for non-contact detection of metal targets in a variety of industrial environments. These low-cost, technologically advanced inductive sensors feature an ASIC (application-specific integrated circuit) programming chip that eliminates production tolerances, enabling the IME to provide highly accurate and repeatable measurements. Using a Hot Melt filling material, IME sensors withstand humid areas and are able to provide excellent shock and vibration resistance. In addition, IME sensors feature a higher tightening torque -- for more rigid installation -- and high immunity to Radio Frequency Interference (RFI) signals, voltage and current spikes (burst, transients), and electrostatic discharge (ESD).

Click to show / hide content block    Web Part Container
Click to show / hide content block  Content Block 02
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
Tracie Manor
6900 W 110th St
Minneapolis, MN
55438 USA
Button to start the search