Search   Start

   SICK-STEGMANN News

All-round innovation and individuality - Flexibility regarding line numbers, improved running properties with vibrations minimised, electrically insulated hollow-shaft terminals, and a maximum operating temperature of +100°C make the new...  more... PDF (83k)
New HIPERFACE® adapter modules for CANopen and DeviceNet - SICK’s rotative, linear and optical position detection systems with a HIPERFACE® interface offer the best bus connections.  more... PDF (103k)
Ace of Trumphs for new quality and economic efficiency - A 16-fold improvement in resolution, an electronic type label and the HIPERFACE interface are the trumps with which the new SEK52 capac- itive encoder is stirring up resolvers in the lower...  more... PDF (111k)
Thousands of adjustments, singular availability - Individual programmability is the strength of the new DRS61 incremental encoder.  more... PDF (95k)
One compact device instead of many components - With the dkV60 incremental measuring wheel encoder, an easy-to-install and economical all-in-one solution for the indirect determination of path, position and speed information is now available.  more... PDF (146k)
Compact class: compact housing, class performance - The new BKS absolute, and PKS incremental, wire draw encoders from SICK STEGMANN are the right choice when reasonably priced and com- pact position and path detection is required.  more... PDF (101k)
DRS61 – the programmable incremental encoder - Waldkirch, October 2005 – Individual programmability is the strength of the DRS61 incremental encoder from SICK-STEGMANN.  more... PDF (54k)
JPEG (423k)
BKS/PKS wire-draw encoders: compact alternatives with 5 m measurement length - Donaueschingen, October 2005 – SICK-STEGMANN has supplemented its programme for position and path determination with the BKS absolute wire-draw encoder and the PKS incremental wire-draw encoder.  more... PDF (56k)
JPG (2491k)
New motor feedback system stirs up “resolver gangs” - Waldkirch, October 2005 – A 16-fold improvement in resolution, an electronic type label, and a HIPERFACE interface are the trump cards with which the new SEK52 capacitive encoder is stirring up the...  more... PDF (52k)
JPG (427k)
DRS61 programmable incremental encoder - Conventional encremental encoder designs can have serious drawbacks for the end user, commodity supplier and system integrator.  more... PDF (815k)
Meypack gets packing - High-performance packaging machines, such as those from Meypack in Nottuln, are characterised by their flexibility and maximum production readiness.  more... PDF (121k)
HIPERDRIVE ® - HIPERDRIVE ® , the integrated positioning drive consisting of a motor, gears, an absolute measurement system, and performance and regulatory electronics, allows rapid automatic product and format...  more... PDF (128k)
Absolut-Encoder ATM 60 - Bronx Taylor/Wilson, English producers of pipe straightening machines, insist on the ATM 60.  more... PDF (98k)
SRM 50 - Unique dynamism, extremely compact housings and high rigidity characterise the new TPM series of geared motors, so-called servo actuators, from WITTENSTEIN motion control GmbH.  more... PDF (121k)
DRS 60-Encoder - Those who use DRS 60 incremental encoders, from the CoreTech series, in their printing and packaging systems can reduce the time required for zero-pulse adjustment by 90%.  more... PDF (85k)
DKS 40 incremental encoder - Predestined for monitoring the rotation of rollers, cylinders and axes   more... PDF (71k)
Format adjustment drive - The „absolute“ positioning drive HIPERDRIVE® as replacement of the hand wheels for format adjustment in machines and plants.  more...
Zero-pulse assignment at the press of a button - The British diesel engine producer Cummins Engine Company is speeding up its engine inspections.  more... PDF (162k)
Contact
SICK Vertriebs-GmbH
Schiessstr. 56
40549 Düsseldorf
Germany

Phone
+ 49 211 5301-0
Fax
+ 49 211 5301-100
SICK World Wide