Skip Navigation Linksexpert-level.com > english > Home > Applications > Machine Tooling
Print

Machine Tooling 
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
Applications in the machine tooling industry 

 

 
 

Hydraulic, pneumatic, cooling and lubricating processes are at the center of almost all automated machinery processes. With modern technology SICK offers increased efficiency to its customers in the machine and tool manufacturing industry with simple and all-purpose sensors.

Click to show / hide content block    Web Part Container
Click to show / hide content block    Content Block 02
Show Content 
No Links 
Show Title 
Show Subtitle 
Show Image 
 

 

Level measurement in washing systems 

 
 

Cleaning plants: SICK's TDR-Level sensor, LFT, continually measures the level of the cleaning fluid. Large or small quantities of foam within the tank do not influence the precise measurement of the fluid level. In addition to the analog signal, the sensor also provides 2 switching signals for use as overfill-and dry run protection.

 

Click to show / hide content block    Content Block 03
Show Content 
No Links 
Show Title 
Show Subtitle 
Show Image 
 

 

CNC machinery 

 
 

Three tuning forks LFV200 detect the maximum-, minimum- and demand level as point level detectors within the coolant container of filter systems. Even dirt and swarf do not influence the rugged measurement system.

The LFT is the ideal choice if continuous level monitoring of coolants is required.

Click to show / hide content block    Content Block 04
Show Content 
No Links 
Show Title 
Show Subtitle 
Show Image 
 

 

Hydraulic presses 

 
 

SICK’s PBS pressure switch is used for continuous pressure monitoring in hydraulic systems, ensuring the machine applies the correct pressure during pressing.

Click to show / hide content block    Content Block 05
Show Content 
No Links 
Show Title 
Show Subtitle 
Show Image 
 

 

Pneumatic presses 

 
 

The PBS pressure switch continuously monitors the pressure within the pneumatic systems of pneumatic presses. This ensures that the correct press pressure is applied during the working process.