LFV200 tuning forks with the option of being completely free of oil-, grease- and silicone are applicable for level monitoring of maximum-, minimum- and demand states in paint shops.
SICKs TDR-Level sensor, LFT, continually measures the level of the cleaning fluid. Large or small quantities of foam within the tank do not influence the precise measurement of the fluid level. In addition to the analog signal, the sensor also provides 2 switching signals for use as overfill-and dry run protection.
SICK’s PBS pressure switch is used for continuous pressure monitoring in hydraulic systems, ensuring the machine applies the correct pressure during pressing.