| |
Seoul now ready to face football’s World Cup
Six months before the start of the World Cup in June 2002, the last of 31 ALIS Airport Luggage Identification Systems went into operation at Seoul’s New Incheon International Airport. The systems are equipped with CLV 295 high-performance bar-code scanners and are used in the transfer and check-in areas. Here, among other things, they will ensure that every team arrives at the right venue in South Korea and Japan with the correct team uniforms and their own football boots.
>> The systems offer a truly champion scoring accuracy. Regardless of how the flight baggage labels on the team bags pass through the reading gate – the bar code is hit accurately with every scanning process. Whether on the strap or in a label-tag – the available space has as little effect on the reading result as the high “speed of play” of the conveyor system at 1.8 m/s.
Fitness constantly monitored
The evaluation PC for ALIS, known as the APC, does not merely evaluate reading results and pass them on, but also continuously checks the fitness of the players involved. The online diagnosis can be evaluated statistically so that, if necessary, a scanner can be replaced by a substitute in good time – before it “runs out of breath”.
|
|