Search   Start
 
Photoelectric Fork Sensors
 
 
These sensors, which function as two-unit through-beam systems, combine a sender and receiver in a single housing. The distance between the sender and receiver is determined by the shape of the housing and is referred to as the fork width.

The emitted light, in the form of a precisely concentrated beam, and the high detection accuracy mean that even minute differences in light attenuation can be detected.

The product groups
WF Next
  • with adjustment via userfriendly keyboard or via teach-in
WF3T / 5T Teach-in
  • for rapid labelling machines
WF Standard
  • with adjustment via potentiometer
 
Photoelectric Fork Sensors
Productfinder
Application