|
 |
DMH Light Section Sensors transmit a laser line, at a defined angle, over objects to be scanned. The laser line hitting the object is then displayed upon a square receiver array as a contour corresponding to the object´s height profile. This allows height profiles to be monitored, newspapers counted, filling levels detected or the alignment of objects to be ascertained and checked for presence. Different integrated software variants mean that the DMH can be quickly implemented for any application. |