You are searching for the optimal reading technology?
We have the answer!
Different from one dimensional or stacked codes that can be read with line or laser sensors easily, a 2D-Code requires a more complex solution. Here a real two-dimensional picture of the code is taken which then is evaluated by special software algorithms. So a 2D-Code reader can be seen as sophisticated image proccesing system.
An optimal solution for 2D-Code reading needs the exact knowledge of all technical requirements like for example contrast ratio or object velocity,. Also cell size, code resolution and depth of field as well as the required reading distance have to be considered. Special challenges are among others optical reflections or bad marking qualities.
As standard technologies there have been come up two reading technics both having their advantages which predestine them for different tasks.
The reading of 2D codes can be distinguished between line or matrix technology. With our products we can offer you solutions for both.
Line:
- high resolution
- identification at high speeds possible
- trigger on object, like with conventional bar code readers
- reading without deformation on curved objects possible
Matrix:
- 2nd dimension automatically integrated
- high depth of field
- user-defined picture area through CMOS technology